Part Number: INA186-Q1 Tool/software: Hi TI team, question regarding current sensor, we have using it in following schematic. VCC = 1.76V VSNS_REF = 0.256V Resistor R3987 10k disconnected IN- shorted with IN+ between 7 and 8 pins. In this setup I should…
Part Number: INA186-Q1 Other Parts Discussed in Thread: INA240-Q1 , , INA186 , INA240 Tool/software: Hi Expert,
Have a good day!
Can INA186-Q1 be used as Inline motor current sense? Just as INA240-Q1:
Thanks!
BRs,
Leo
Part Number: INA186-Q1 Hi expert,
I found that the settle time only have typical value 30 us, since we expect software calibration this value, could you pls check what the min and max value for Setting time? and If there is a defined peripheral circuit…
Part Number: INA186-Q1 Tool/software: Hello,
I would like to ask If I can apply 0V to +16V respect to GND on Vin+, Vin- pins, if INA´s VS pin has 0V against GND (INA is not powered)? Thank you
Part Number: INA186-Q1 Tool/software: Hello,
Could you please help me understand what would be the difference in functionality if we use 10R or 100R along with 220pF capacitor as an RC Filter at the input of IN- and IN+ Line.
I want to understand…
Part Number: INA186-Q1 Other Parts Discussed in Thread: INA186 Hi expert,
If we test a current signal of 0.5ms to 2ms with INA186, could you help evaluate the output response time?
1.Is the signal distorted
2. Is there a delay in the signal, and…
Part Number: INA186-Q1 Other Parts Discussed in Thread: INA212 Tool/software: Hi expert,
My customer want to use a Current-Sense Amplifier to trigger 3.0A current with a 0.2mΩ shunt resistor, and they thought the gain is not enough. Do we have more…
Part Number: INA186-Q1 Tool/software: Hi team,
I see the gain error of INA186-Q1 is 1%, however I did not see total error.
Customer compared INA186-Q1 with INA194-Q1, they saw INA194-Q1 has 3% total error.
They want to know the total error of INA186…
Part Number: INA186-Q1 Other Parts Discussed in Thread: INA186 Tool/software: Hi Expert,
Have a nice day!
For INA186A1-Q1, its bandwidth is 45kHz. So, what is the max frequency AC current INA186A1-Q1 can detect? Can it detect 20kHz current?
…
Part Number: INA186-Q1 Other Parts Discussed in Thread: INA186 Tool/software: Hi Expert,
Customer is using INA186A2QDCKRQ1 in current sensor application. The waveform is described as below and pls ignore the green line and red line. When the current…