Part Number: INA194A-Q1 Tool/software: Hi Team,
May I know how to judge whether INA194AQDBVRQ1 can be washed with AQUANOX A4625 (Cleaning Solution ) ?
Thank you.
Part Number: INA194A-Q1 Hi Expert,
My customer is using our INA194AQDBVRQ1 in their HUD project.
The OEM is asking for the CTE value of this device. Could you please check the CTE(coefficient of Thermal Expansion) value of INA194AQDBVRQ1 ?
Thanks…
Part Number: INA194A-Q1 Other Parts Discussed in Thread: INA194 the output of INA194AIDBVT error and its up to 3.3v, the power supply of INA194 is 3.3V.
in our designer, the sensor resistor is 50mR.
Only one abnormal chip has been found so far, so…
Part Number: INA194A-Q1 Other Parts Discussed in Thread: INA293 , INA194 , INA290 , INA281 , INA280 Please let me know if there is accuracy better than the INA194AQDBVRQ1. Also, if there is an isolated current amplifier that is inexpensive and has good…
Part Number: INA194A-Q1 Customer found an abnormal waveform when using the INA194A device on H-Bridge MOSFET application.
application: AC inverter.
Issue Description: There are two INA194A to sensing the motor current in bidirectional. When motor…
Part Number: INA194A-Q1 Other Parts Discussed in Thread: INA194 hi there,
my customer wonders which maximum values for the Analog Inputs, Vin+ Vin- on INA194A-Q1 apply. the datasheet of INA194 lines out -18 to +18V ; in the datasheet of INA194A-Q1 this…
Part Number: INA194A-Q1 Other Parts Discussed in Thread: INA240 , INA293-Q1 , INA240-Q1 Hi, Sirs,
We are using TI current sensor INA194AIDBVR. The architecture is as follows.
We would like to sense the current of DK_36V_OUT. The DK_36V_OUT is 36V…
Part Number: INA194A-Q1 Hi All,
My customer has a question about slew rate.
The dataSheet has a TYP value of 1 V/us.
However, there is no description of the minimum value.
What is the minimum value?
Best Regards, Koji Hayashi
Hi Patrick-san
Thank you for response.
I understood as follows.
The differential impedance between the input terminals.
INA240-Q1 is 3.2kohm.
INA194A-Q1 is 5kohm.
Current limit on all pins
INA240-Q1 is not clear.
INA194A-Q1 is 5mA…