Part Number: INA196 Other Parts Discussed in Thread: LM5069 , , INA303 , INA302 , INA301 I want to know if it is possible to share the shunt of the LM5069 for an inrush current protection with an INA to monitor the used acutal current.
i do not like to use…
Part Number: INA196 Hello
I want to interface pressure sensor using INA196, my sensor works on 24v. I'm attaching circuit please let me know is it correct?
Can differential voltage be 16V?
Part Number: INA196 Other Parts Discussed in Thread: INA138 , TIDA-00332 , ISO1541 , TIDA-00313 , INA226 , ISOW7842 , INA260 Hi,
The common mode voltage of INA196 is limited to 80V.
How can I extend the common mode range of INA196 to measure a 110V DC rail…
Part Number: INA196 Other Parts Discussed in Thread: INA195 Hi
My client is currently applying INA196.
Make sure that there is no abnormality in the connection of the current detection part of the circuit.
The INA195 detects the current flowing in the…
Part Number: INA196 Other Parts Discussed in Thread: RCV420 Hello,
I need to 4-20mA current loop to voltage converter IC. Can I use INA196? It says it is high side sensing device. For my application the input 4-20mA current loop comes from external sensor…
Part Number: INA196 Other Parts Discussed in Thread: INA240 Hi,
The INA196 have bandwidth of 500KHz according to the datsheet. I need to measure the current on an AC rail with 12V @ 200KHz switching.
Q1. Can I use INA196 for this purpose?
Q2. If Yes, Do…
Part Number: INA196 Other Parts Discussed in Thread: INA195 Hi there !
In the datasheet, under Absolute Maximum Ratings the input voltage is given with -+/ 18Volts. How can the common mode voltage then be -16/ + 80 volts ?
Thank You !
Other Parts Discussed in Thread: INA196 Hello,
i have a Problem with a ina196.
My measurements show that this must be a 100V/V (for example a 198) instead 20V/V Type.
The Part show's the Sign
| - -
| B J E
| - -
Can anyone affirm this as…
Part Number: UCD90120A Other Parts Discussed in Thread: INA196
In our latest design, we use MON2 to sense current from INA196. I break the link between INA196 and MON2, and measure the voltage of the INA196 output and MON2. But there's abnormal pulse…
Hello Chien,
I cannot see a clear reason why you are getting such large errors. Can you share the output voltage you are measuring? Also how are you getting the output voltage of the INA196? Is it from the ADC of the UCD9090? If so can you measure with…