Part Number: INA200-Q1 Other Parts Discussed in Thread: INA200 Hello Support team,
I can find the below typical application in the datasheet.
According to Table 1,
V OUT_TRIP = I TRIP x R SHUNT x Gain = 1A x 5mΩ x 20V/V = 0.1V
R2 / (R1+R2…
Part Number: INA200 I have an INA200 whose output voltage is at the max Vs rail regardless of the load current. This is the first time I have seen this behavior on otherwise working hardware - there is significant run time on the system. The power supply…
Part Number: INA200 Hi, team.
I have a question about INA200's behavior.
Please tell me.
<Question>
Q1:I think that CMPOUT goes H when the CMPIN terminal voltage of INA200 is below 0.6 V, is it correct?
Q2:If the Q1's answer is "Yes", I think…
Part Number: INA200 Hi, team.
I posted the following thread.
e2e.ti.com/.../732488
Let me confirm CMPout behavior on INA200.
<Quesiton>
While Vin keeps Low (<0.6V), does CMPout keep Low even if RESET repeat High and Low?
On my customer…
Part Number: INA200 Regarding section 7.3.3 of datasheet:
What rise time is appropriate for a 5V reset?
The datasheet didn't specify, so I chose 1ms(seems wrong now). The CMPOUT pin floats at 2V on power up. Is this due to a bad rise time choice?
Part Number: INA200 To whom it may concern,
This is for automated test equipement.
I want to use INA200 to monitor current of DUT(device under test), and disconnect(by relay) the DUT from circuit if current draw exceeds 20mA, and also turn on a…
Part Number: INA200 Other Parts Discussed in Thread: INA293 Hi Team,
Would you advise my customer's question below?
Since the pattern coming out of the out pin is very long, I would like to add a
1000pF capacitor between OUT and GND to remove noise…
Part Number: INA200 When there is a rising edge on Signal #REST the Output CMPO goes high without any current through the shunt.
After this a high low high on Signal #REST will reset the Output CMPO.
But the next rising edge on Signal #REST the Output…
Part Number: INA200 Other Parts Discussed in Thread: INA240 Hello Team,
I'm actually working on an OCP function, in a system where the common mode voltage can vary from 0V to 48V. As the commutation of common mode voltage is realised thanks to FET,…
Part Number: INA200 Other Parts Discussed in Thread: INA240 Hello Team,
My customer use our INA200 for high side current detection, If the input signal common mode is square wave as below, it is OK of this application? Thanks
Regards,
Nanfa…