Part Number: INA206 Hello Support team,
Is it possible to make INA206 disable state by "RESET"?
Is the function of "RESET" just only clearing the latch of "COMP OUT"?
Best Regards,
Hirokazu Takahashi
Part Number: INA206 Hi sir,
I want to use INA206 in my new design.
I can find 4 resistors in internal block diagram.
8.2 Functional Block Diagram
https://www.ti.com/lit/ds/symlink/ina206.pdf
Can you tell me each resistor value and each resistor's precision…
Part Number: INA206 Hi Guys,
i have a question of "Is the current bi-directional or uni-directional?"
Requires an additional input to determine current flow direction
-Vout > VREF --> the system is sinking current
-Vout > VREF --> the…
Part Number: INA206
I am using INA206 at high side for overcurrent threshold monitoring. The load is supposed to draw 4 - 4.5 A current. I have set the overcurrent threshold at 4.7A using the Comparator 2. Now I am facing two issues while testing this…
Part Number: INA206 The datasheet of INA206 specify the operating supply range from 2.7V - 18V, however the device shows unusual behavior when powered from a 3.3V source i.e. comparator's output does not go high when it is expected to. The same circuit…
Other Parts Discussed in Thread: INA203 , INA206 Hi,
Could you please tell us the technical difference between INA203 and INA206 although these parts are the current-shunt monitor with dual comparators ?
Best regards, Kato
Other Parts Discussed in Thread: INA206 Hello, I have a question about INA206.
I attach a circuit.
INA206.pdf
Please teach me the connection of three GND of red circle. Should GND connect to the GND? Should GND connect to the AGND? Should GND connect to the…
Other Parts Discussed in Thread: INA206 , INA208 , INA207 Hello,
We are planning to use the INA206. However, we are a bit confused what is meant by "latch" in the data sheet? The follow is from the datasheet.
The INA206, INA207, and INA208 devices…
Other Parts Discussed in Thread: INA206 , TLV3404 I am using an INA206 operating at 5V. The comparator output pin is pulled up to 40V through 160k. I overlooked that absolute max voltage on comparator outputs is 18V on the datasheet.
On the actual hardware…
Other Parts Discussed in Thread: INA381 , INA193 , INA200 , LMP8601 , INA282 , INA206 , TMCS1100
Hi,
I design Pulse generation circuit using Op-amp.
Without current sensing amp(INA381), the output signal is no problem.
But, add current sensing amp(INA381),…