Part Number: BQ25703A Other Parts Discussed in Thread: BQ25703 , , INA208 Hi,
we are using BQ25703 for our embedded system and would like to have a simple LED indicate charging.
I see IBAT pin which is 8, 16 x the current. Would a simple external comparator…
Other Parts Discussed in Thread: INA206 , INA208 , INA207 Hello,
We are planning to use the INA206. However, we are a bit confused what is meant by "latch" in the data sheet? The follow is from the datasheet.
The INA206, INA207, and INA208 devices…
Other Parts Discussed in Thread: INA169 , INA205 , INA202 , INA198 , INA286 , INA195 , INA283 , INA208 Hi:
I would like to measure 10mV to 50 mV shunt at 60VDC max resulting in linearly proportional output voltage from 0 to 5VDC in a telecom battery plant application…
Current sense amplifiers are different from typical op amps and instrumentation amps because the common mode of the inputs can exceed the supply rail of the device. These amplifiers have different architectures to make this happen, and part of the way…
I tried one unit in the lab just now and found that with 5V supply and nothing on the inputs, I measured roughly 1.6V on VIN+ and VIN-. I swept the Vs around from 3 to 7 and saw the voltage on the inputs change from roughly 1.5V to 1.7V. Also, there was…
Yoshihiro-san,
Unfortunately we are unable to provide data like that to a customer without an NDA. I can confirm that the data sheet parameters are an accurate representation of the data. The offset voltage is better than ±3mV over 25°C to 125°C, and…
Other Parts Discussed in Thread: INA207 I am using the INA207 as a replacement of the MAX4375. Its larger input voltage range is an advantage and we started using the INA207 as a product replacement and for new designs. The exact part number I am using…