Part Number: INA210-Q1 Other Parts Discussed in Thread: INA210 , INA187-Q1 , INA190-Q1 , INA186-Q1
Hi Expert,
My customer is doing test with INA210-Q1, here is their system:
They short the LV to LV_GND, which leads to a -1.5V to the IN+, the output…
Part Number: INA210-Q1 Other Parts Discussed in Thread: INA210 Tool/software: Hi,
My customer is INA210-Q1 and have several questions to ask.
Under normal circumstances, the current flowing through the shunt resistor of our product is about 65A~75A…
Part Number: INA210-Q1 Tool/software: Hi team,
could you help to check what value is the minimum capacitor on V+ pin, from the datasheet, I see the value is 0.1uF. if we can use <0.1uF capacitor(total)?
Part Number: INA210-Q1 Other Parts Discussed in Thread: INA210 Tool/software: Hi team,
customer change the RS from 10 ohm to 1000ohm, we know the resistor would make large error. but we can't understand it - the output is correct when the current flowing…
Part Number: INA210-Q1 Hi Team,
Just curious that compare with SC70 package why did the UQFN package has two pins of IN+ and IN-?
The customer should connect 2 and pin3, pin4 and pin5 directly, right? Is there any thing need to notice when they…
Part Number: INA210-Q1 Our customer has a question about V+ voltage range when his circuit apply 10VDC VIN+ Bus Supply. Is it available if INA210-Q1 can support from V+=2.7V to 26V range.
best regards,
Part Number: INA210-Q1 Other Parts Discussed in Thread: INA210 Hello,
Our customer is asking how to connect REF pin in case INA210-Q1 is used as positive half wave current on the rails.
Do you recommend to connect REF pin to GND in this case ?
In…
Part Number: INA210-Q1 Other Parts Discussed in Thread: INA213-Q1 , , INA210 , INA190 , INA191 , INA186 I would like to know about your part INA213A-Q. Our requirement is to sense 0-50mA. we are using your part INA210-Q1 /INA213-Q1 for our application…
Part Number: INA210-Q1 Hi team
INA210-Q1 D/S say Input bias current = Max 35uA .
[1] so total input bias current would be Max 70uA(= 35uA x 2) for two input pins ?
[2] further, may I know total input bias current for two input pins at Vs = 0V…
Part Number: INA210-Q1 Hello,
On using Pspice model INA210-Q for doing simulations in SIMETRIX, I'm not getting the result at temperature 85 degree Celsius. The following error is shown. Could you please provide model that can go up to 85 degree Celsius…