Part Number: INA2126 Other Parts Discussed in Thread: REF5030 Hi to all!
I need to capture two signals from two load cell, so i did a circuit with an INA2126 to amplifying this signals and acquiring they with an adc. This is my circuit
The load cell is…
Other Parts Discussed in Thread: INA2126 , INA126 Dear all,
This is my first time on this support. I am a dutch student.
I have a INA2126 instrumentation amplifier used to amplify the results of a load cell. I supplied the amplifier with 5VDC and I have…
Other Parts Discussed in Thread: INA326 Hello everyone.
I have been trying to get this instrumentation amp to work for a few hours now and I have no clue what I am doing wrong. I am using a function generator to input a sine wave (~20mVpp, 500Hz) into…
Other Parts Discussed in Thread: INA2126 , INA333 , INA326 , ADS1247 , ADS1118 , ADS1220 I'm trying to amplify the voltage from an RTD (resistance temp device) using one amplifier on INA2126 using a single 5VDC supply. The circuit is attached. The 0.1VDC voltage…
Other Parts Discussed in Thread: ADS1211 , INA2126 , REF5025 Hi All,
I'm doing project on weigh scale application.
I'm using ina2126 and ads1211 in the analog part and im using one smps.
I'm getting following problems.
1. I'm not geting the stable…
Hi Claudio,
We have not been able to reproduce the problem using our own setup.
We put a LIB file into a read-only directory called "lib" and include that LIB file in our simulation profile:
Then we closed the project and reopened it and here…
Hello Skippy,
The INA125 is the only instrumentation amplifier that has an integrated bridge reference. It only comes as a single device.
The only dual instrumentation amplifier that comes in a DIP, or through-hole, package is the INA2126.
If the…
Cole,
Thank you very much. That explains it and the tool is great. I wish I would have known this earlier, I originally just used the data sheet and the graph of the common mode range looks like my conditions are within the window of accepted operation…