Part Number: INA214-Q1 Other Parts Discussed in Thread: INA214 Dear team,
In our datasheet mentioned gain error is related by both internal resistor as well as external resistor. According to the simplified calculation of error factor, how should I define…
Part Number: INA214-Q1 Hi expert,
My customer find some issue about Ref pin floating or give it a 3.5kohm will see the output signal have 10khz abnormal noise as this pic
their original circuit connect is Ref pin and Gnd pin connect together then connect…
Part Number: INA214-Q1 Other Parts Discussed in Thread: INA240 hi team,
now my customer want to use INA214-Q1 to sense the current of motor, The motor speed is based on 100rpm, current sampler scheme, phase current frequency is approximately 14Hz, PWM…
Part Number: INA214-Q1 Other Parts Discussed in Thread: INA214 Hi team,
In INA214 ds, the maximum capacitive load is 1nF. if customer use RC at output (100ohm 0.01uF), do you see any issue?
Another question is how to calculate the bandwidth in their case…
Part Number: INA214-Q1 Other Parts Discussed in Thread: INA214 Hi,
Can you provide a complete, detailed list of differences between INA214-Q1 and INA214,the customer will schedule the test based on the point of difference,thanks
Part Number: INA214-Q1 Hi Expert,
As said in datasheet, INA214-Q1 has fixed gain. But they choose large Rs, such as 10Kohm. So the calculated gain error would be very large, near to 90%. Then they use Gain_real= 100*(1-90%)= 10 as the real gain simply…
Part Number: INA214-Q1 Other Parts Discussed in Thread: INA228 , INA214 Dear team,
My customer feedbacks that 100uV offset voltage is too large for them. They hope the offset voltage can be pV or nV level. Do we have such devices?
Thanks & Best Regards…
Part Number: INA214-Q1 If the V+ voltage is 15V + (+/-500mV) ripple. For example, what is the impact on gain errors? Because there is only the influence of Gain vs Temp in the specification, there is no influence of Gain vs V+.
BR, Gary
Part Number: INA214-Q1 Other Parts Discussed in Thread: INA214 Dear team, I'm using the INA214-Q1, in the configuration below, for measure the output current of a 0,85V power supply with 2A of nominal current. I made some tests with a Rshunt=7mohm and…