Part Number: INA2143 Tool/software: Hi,
I have a customer using this device, they were wondering if there's any newer alternatives they should be aware of? Thanks!
Part Number: INA2143
Hi Team,
The customer would like to know the difference between INA2143U and INA2134UA. I see the performance parameters on page2 and 3 of the datasheet
for INA2134UA are shown " * ".
What is the difference between INA2143U…
Other Parts Discussed in Thread: INA2143 , OPA548 , INA143 , INA106 Hello,
I am using a INA2143U for a current measurement circuit. (sense resistor = 0.1 Ohm, load = 1mH, 10 Ohm).
Measurements show that the INA2143 is not linear: for frequencies higher…
Other Parts Discussed in Thread: INA2143 I have a customer who is using the INA2143 and has a question related to leakage. Customer would like to know on Input pin N+ and N-, how much leakage current is there on the pin?
Part Number: AMC1311 Other Parts Discussed in Thread: INA2143 , , AMC1350 , AMC3330 Dear Sir and Madam,
I am currently designing an isolated amplifier circuit, that is capable of measuring a high voltage signals up to 1500 V with at least of 20 kHz…
We have instrumentation amplifiers with gain of 0.1 but only up to 5.5V single supply: see INA326/7 and INA336/7. However, for 12V direct battery monitoring, you will need higher supply voltage - in such case, we can only offer difference amplifiers like…
Hello Carlos,
The THS4521 is a good driver, and it should be able to drive many differential ADCs.
Besides, we have two different options so far for this project with differential inputs drivers. In order to make an input single ended, the negative…