Part Number: ADS7138 Other Parts Discussed in Thread: INA2191 Tool/software: Hi,
i am using (LT1790 max 5mA) for 4.096 reference of ADS7138. Since i also had INA2191 suitable for this line, i have added it on 4.096 reference.
I am little concerned…
Part Number: INA191 Other Parts Discussed in Thread: INA199 , INA2191 , INA241A Tool/software: Hello,
In existing design we are using AZ-0500 1:500 (Talema) current transformer and TLV9002ID* to measure 400VAC 50/60Hz
Primary current range: 62.5mA…
Other Parts Discussed in Thread: INA190 , INA191 , INA186 , INA2191 Hello,
I need a way to measure low current on a negative voltage -24V.
I there a way to connect a current sensing amplifier for this negative common mode.
The parts I found are…
Other Parts Discussed in Thread: INA190 , INA2191 Hi, TI Support Team
Please recommend a product capable of current sensing with the following spec.
Sensing current : 0~1.4mA
input Voltage : 5V
Please recommend a product with high accuracy.
…
Part Number: INA190 Other Parts Discussed in Thread: INA228 , INA229 , INA121 , INA2191 , INA238 , , LOG114 Hello TI Team,
I have to measure the current in Micro ampere range and also in the Ampere range. Should I have to include two current sense amplifiers…
Part Number: INA4181 Other Parts Discussed in Thread: INA186 , INA2191 , INA4290 , INA280 , INA281 Hi TI experts, I was using INA4181A2IPWR and found that it has a large power consumption after shutting down. The test is as follows. IN+1 and IN-1 are…
Part Number: INA191 Other Parts Discussed in Thread: INA2191 , INA2181 Hi,
I am planning to use this device with a shunt resistor for measuring a 54 V battery current. Would it be any problem if I do this measurement in the negative terminal of the…
Other Parts Discussed in Thread: INA190 , INA237 , INA186 , INA2191 , INA228 Hello,
I need to sense a current for AC system - charging/discharging of the Capacitor.
Do you have any current sense amplifiers that support AC signal 20Vpp and can sense…
Part Number: INA190 Other Parts Discussed in Thread: INA2191 , INA191 Hi,
I have an application that uses 19 INA190A2 differential amplifiers and need to bias the VREF pins so that the amplifier output voltages keep the ADC in the linear range over…
Part Number: INA2180-Q1 Other Parts Discussed in Thread: INA2180 , STRIKE , OPA2192-Q1 , OPA2192 , INA2290 , INA2191 Dear expert,
Customer is using INA2180A3-Q1 for high side current measurement. Vbat is 9V~16V. Current is from 1A~30A. Current sensor…