Part Number: INA220
As mentioned earlier query , the ADC is powered off the voltage as Vs pin. All level shifting of the shunt voltage from VCM to ground level for internal ADC is done internally. All error effects from power supply (PSRR), VCM (CMRR…
Part Number: INA220 Other Parts Discussed in Thread: INA237 Hi Ti FAE,
I'm in charge in OpenBMC FW development from inventec company.
We use inv220B for fan power/current/voltage monitor.
and need TI confirm/review the inventec's implemented/progress…
Part Number: INA220 Hello, At datasheet Figure 31, in addition to the load current, the current to the 13.7kW also goes through the Sunt resister. To measure only the load current, my customer thinks the connection should be as follows by right. Does…
Part Number: INA220
Hello,
Can you please assist with finding a datasheet for this PN? The INA220 datasheet I find on ti.com does not call out this specific PN and the pin count differs from the datasheet as well (14 pins vs. 10). We have a customer…
Part Number: INA220 Hello,
I'm trying to write the calibration register (0x05) in u-boot i2c tool, and I can't seem to get it to work properly. I've tried all different syntax, but u-boot seems to want to write one byte to the address, and the…
Part Number: INA220-Q1 Hi Sirs,
I don't have experience to set I2C address by connect to PIN SCL,SDA before.
Will it make any problem if I connect the A0, A1 to SDA and SCL directly or connect the A0, A1 to SDA and SCL through 0ohm resistors?
Thank…
Part Number: INA220-Q1 Other Parts Discussed in Thread: INA220 , INA228
Hi ,TI team
The below is the input sense voltage range as in below table for INA220. For various PGA modes ( 1 to 8) as enclosed from data sheet table 7.5
We want to measure current…
Part Number: INA220 Dear team
The customer would like to simulate the thermal, I can't find some parameter about thermal. Could you help to provide the parameter as below.
Critical Component
Description
Power consumption in normal operation PD (Watt…