Part Number: INA226 Tool/software: Dears,
Recently, the current monitoring of INA226 in the customer's radar equipment failed. The current value read was fixed at 8192mA, and the actual value should be within 20mA. After replacing the new INA226, the…
Part Number: INA226 Tool/software: The datasheet shows the input impedance of Vbus is 830K. in current detection mode from the shunt resistor, will the input current of Vbus be I=V/830K or what's the input current of Vbus in current detection mode …
Part Number: INA226-Q1 Other Parts Discussed in Thread: INA225-Q1 , INA237 , INA238 , INA228 , INA234 , INA236 , INA232 , INA4230 , INA4235 , INA223 , INA190-Q1 , INA225 Tool/software: Hi team,
I want to know why most of our digital power monitors have only 1V/V…
Part Number: INA226 Other Parts Discussed in Thread: INA230 , CS-AMPLIFIER-ERROR-TOOL Tool/software: Hi team,
Could you kindly help provide a detailed comparison between the INA226 and INA230 based on the worst-case scenario, considering offset and gain…
Part Number: INA226 Tool/software: Hello,
I noticed that input bias current of INA226 has recently been updated on the datasheet revision B.
- Decreased input bias current typical value - Updated Shunt Input Gain Error vs Common-Mode Voltage graph and…
Part Number: INA226 Tool/software: Hi Team, We were designing a VI monitor for a 200V system and came across this reference design. I had a few doubts regarding this: "The INA226 can also sense bus voltages less than 36 V. Since the bus voltage employed…
Part Number: INA226-Q1 Other Parts Discussed in Thread: INA226 Tool/software: Hello team,
Is there any situation will cause abnormal I2C communication between the host and INA226: no response to the host (either ACK or NAK) for a long time, and the I2C…
Part Number: INA226 Tool/software: Hello
I want to monitor current of the load,
INA226 can be measured the below current spec. ?
Required Spec.
1. Current sesnsing Range : 200 uA ~ 500mA
2. DC Power : 12 V
Thanks.
Part Number: INA226 Other Parts Discussed in Thread: INA149 Tool/software: Hi Everyone,
I need to measure DC current bidirectional max ± 10A and searching best solution about it.My accuracy need to ± 5 ma.
Now i don t need to voltage measurement…