Part Number: INA226 Hi guys,
I have a very strange experience with inexpensive ina226 modules.
I have pretty simple usecase, where I only need to measure the bus voltage Vbs. I don't measure the current.
I ordered several pieces of inexpensive ina226…
Part Number: INA226 Other Parts Discussed in Thread: INA228 , INA229 , INA237 , INA239 , INA238 Hi team,
My customer use INA226 to measure mA level solution.
Currently they would like to measure nA level, so do we have any suggestion?
Thanks
Part Number: INA226
From our customer we would like using INA226 for voltage detection to make sure voltage is not over the tolerance when system operating.
From your opinion, we should set total tolerance or DC tolerance?
In other words, is INA226…
Part Number: INA226 Dear team,
I'm reaching out for advice for the appropriate way of VBUS connection, I found that DS recommend connecting VBUS to IN+ or IN-, but there is a suggest said if VBUS connect to SENSE network, will impact the whole power…
Other Parts Discussed in Thread: INA226 , AMC1400 我需要检测电流,使用了75MV分流器,INA226可以精确的测量,然后通过隔离I2C传输。但是系统上了1500V,我想知道AMC1400是否适用?AMC1400范围250MV,在75MV上,前级输入误差会不会太大。哪种方案更好?是否有75MV的隔离放大器?
Part Number: INA226 Necesito una guía paso a paso para importar los modelos Pspice de Ti a OrCAD 17. Estoy particularmente interesado en el INA226 estoy haciendo un proyecto donde necesito simular y diseñar un PCB, pero cuando entro a la pagina el modelo…
Part Number: INA226 Hola, lo que sucede es que estoy descargando el modelo de simulación del INA226, pero cuando lo descargo me aparece un archivo.
pero no sé cómo convertirlo en orcad para que me aparezcan los archivos(.olb y .lib) Si alguien…
Part Number: INA226-Q1 Other Parts Discussed in Thread: INA226 Hello,
I2C can communicate correctly, MCU is master, INA226 is slave.
when WRITE, the HDDAT time (from SCL pull down to SDA jump time) measured by oscilloscope was 1.712us. However, the HDDAT…
Part Number: INA226-Q1 What is the maximum pull up voltage that can be applied to the alert pin of the INA226-Q1? The datasheet seems to imply 6V but I was wondering if it could be pulled to a higher voltage, ie, 28V?