Part Number: INA228 Other Parts Discussed in Thread: SYSCONFIG , DAC53202 I'm trying to connect INA228 with nRF52840 is that possible. Any reference's if possible
Part Number: INA228 Hi, I have an INA228 and I want to set it up correctly. However, all the combinations I've tried seem to be wrong. I would love it if you could explain to me how to correctly connect the load, as well as where to connect the inputs…
Part Number: INA228
Hello
I have a setup utilizing the EVM of INA228.We soldered a 25 mOhm Rshunt and connected an electronic load to the load part, with a VBUS of 5V.
We are encountering two issues that we are struggling to understand.
Firstly…
Part Number: INA228
Hi,
I want to delve deeper into the calculations happening on the monitor. Where can I find this information?
Thank you in advance.
Part Number: INA228 Hello!
The doc for the INA228EVM (shou241e.pdf) in section 4.2.3 says " Connect a shunt resister by doing either of the following: a. Solder a 2512 resistor across the pads of R1 that connects the IN+ and IN– inputs b. Connect an…
Part Number: INA228 Other Parts Discussed in Thread: INA229 Hello! I just got an INA228EVM board with SCB. I have loaded the SBAC253A serial and cloud drivers on a Win 10 PC, and the board shows up in Device Manager as Com7 which I set to 115k or 9600…
Part Number: INA228 I'm currently using INA228 EVM with SCB connected with it. After GUI showing the status of "device connected", pop up message showing "firmware update required". After selecting "load firmware" option, 4 LEDs (D1, D2, D3 & D4) on SCB…
Part Number: INA228 Other Parts Discussed in Thread: SYSCONFIG I'm currently doing a project which involves having to measure the shunt voltage with the INA228EVM and read this into a python script.
However, when I try following the user guide (page…