Part Number: INA229-Q1 Other Parts Discussed in Thread: INA229 , INA233 Team,
is there a feature that allows to check the integrity of the SPI messages sent from the device to an MCU?
My customer needs to have this since the INA229 is located in some distance…
Part Number: INA229 Other Parts Discussed in Thread: SYSCONFIG
Hi expert,
I would like to confirm with you that if the Current Regisiter reading is 0F FF FC (This is the value that has been shifted right by 4 bits), it corresponds to a large current…
Part Number: INA229-Q1 Other Parts Discussed in Thread: INA229 I'm using the INA229 in a battery system which can reach up to 80V when fully charged. Since this is close to the maximum allowable common mode voltage or Vbus voltage of the device, it is…
Part Number: INA229 Other Parts Discussed in Thread: INA226 , INA228 Can I configure the chip to measure -5V power supply? Is there a reference circuit that I can follow? Thanks!
Part Number: INA229 Other Parts Discussed in Thread: SYSCONFIG Hi Team,
A customer is asking about how to interface a Raspberry Pi to INA229 and TMP to analyse the incoming data from these sensors and make decisions (like switching action using a solid…
Kang Andrew said: I was able to read the correct value by reading and writing with 8 bits.
I did forget to mention that in 8-bit configuration, you will need to shift the byte address << 8 before writing to the SPITXBUF. It looks like you may have figured…
Part Number: INA229 Other Parts Discussed in Thread: INA228 Dear team,
My query is regarding INA229 of the Amplifier category of Texas Instruments.
Can I make use of daisy chain connection configuration to connect multiple INA229 to my Raspberry Pi 4…
Part Number: MSP430F5636 Other Parts Discussed in Thread: INA229
Hi,team
My customer has the following questions:
“Hi, In MSP430F5636IPZ. How do I make connections for RTC_CLK (Pin 88) the datasheet says it's a digital i/o pin , should I connect it with…
Part Number: INA229 Other Parts Discussed in Thread: TIDA-00302 Hi all,
I'm going to use the INA229 as lithium battery power monitor in low-side style but I'm worried about the low common mode input range of the pin IN+ and IN-.
In a situation…
Part Number: INA229
Hi Team,
I'm using INA229 to measure current, voltage, power, and temperature of four 12V 100Ah batteries connected in a series-parallel combination. Does the INA229 only measure
1. Die temperature/Internal temperature of the…