Part Number: INA232 I'm using 8 INA232A units on 4 I2C busses, half at address 0x40 and the other half at address 0x41. I can only communicate with those at address 0x41, and I'm not sure why. I'm only trying to read the device ID but again, only those…
Part Number: INA232 Other Parts Discussed in Thread: SYSCONFIG Tool/software: Hi community, I am working on the integration of INA232 sensor in linux kernel. I see that updates should be applied on the drivers/hwmon/ina2xx.c to get the support of the…
Part Number: INA232 Hi
If the INA232 only has IN+/IN- pins and no VBUS voltage, can it measure the actual voltage?
If the INA232 can measure the actual voltage, how should the IN+/IN pins be connected?
And can the maximum measured voltage be 48V…
Part Number: INA232 Tool/software: Hi expert,
This is general question about I2C but I would like to understand following points,
- Once miss communication due to noise or other reasons was happend, Do we have any recommendation to recover this…
Part Number: INA232 Other Parts Discussed in Thread: INA230 , Hi E2E,
I'm using CS comparison and error tool but it is not working on our latest MS office.
Could you replace it with newer version or help me to calculate the error under this particular…
Part Number: INA232 IC should be placed close to the object which we want to check the current value.
Is it ok if the object is placed far to the IC?
Is there any suggest distance between object and ic?