Part Number: INA2332 Other Parts Discussed in Thread: INA2331 , I have an amplifier circuit that is configured to use an INA2332 Instrumentation amplifier. Can I use the INA2331 as a drop-in replacement?
As far as I can tell from the datasheet the INA2331…
Hi Kumar,
Is it abnormal that the offset voltage is almost 41% of the output signal?
When you short the inputs of INA2332-A and INA2332-B port, you Vout_offset_Rx = 151.53 mV and Vout_offset_Rcomp is 11.042 mV. Since you gain is configured at 100, Vos_A…
Hi Atharv,
yes, you can do that. But as being a micropower instrumentation amplifier the INA2321 shows considerable higher noise. This can be an issue when chosing a high gain. Also, for the same reason, the INA2321 is not as fast as the INA2332.
Kai …
Part Number: INA2332 Other Parts Discussed in Thread: INA2331 , INA332 , INA122 , LM7705 I'm using a INA2332 for reading a diferential voltage from a bridge. When the diferential source is 0 (short-circuit), in the output I have 65mV, even when amplifier…
Part Number: INA2332 Other Parts Discussed in Thread: INA332 Hello,
I'm seeing a strange thing when trying to use one circuit of an INA2332 to measure the differential voltage generated by a thermocouple. If I replace the thermocouple with a short…
Part Number: INA2332 Hi everyone,
I am having some problem with output with the INA2332 based bridge amplifier. Differential inputs(pin2 of all Header3) are connected together with one bridge circuit using Variable Resisters. Common mode voltage is 2.5V…
Other Parts Discussed in Thread: OPA2340 , INA2332 , LM3940 Hi everyone,
I am having some issues with noise with the INA2332 or the OPA2340. Would anyone knows where this noise comes from?
Thanks in advance for your kind help.
Other Parts Discussed in Thread: INA2332 Dear ladies and gentlemen,
I'm using your INA2332 amplifiers in an application with 8 load cells (with 260 Ohm strain gages). The gain is set to 1000 with Rin=5k1; Rf=1M on all amplifiers, supp. voltage=5V. To…
Other Parts Discussed in Thread: INA2332 I am using INA2332 with a single supply of 5V.
The input to the op amp is a thermocouple output in the range of 0 to 50mV. The gain is set to 20.
My circuit works fine when Vref is grounded or set to a value of…
Other Parts Discussed in Thread: INA2332 Hi,
I need to measure a voltage on a coil and enter it to the input of the INA2332.
The coil is charged from a differnet source.
Do i need to apply a resistor in parrallel to the coil and than to connect it to the…