Part Number: INA234 hi,
in the datasheet mentioned that current sensor supports both configurations: High Side Shunt and Low side Shunt - could you please explain pros and cons of both config ?
thanks
Part Number: INA234 Hi expert,
Customer measured t(low) = 1.23us in fast mode which is lower than DS minimum spec requirement 1.3us but no any communication issue.
Is it acceptable or any concerns?
Regards,
Allan
Part Number: INA234 Other Parts Discussed in Thread: SYSCONFIG Hello Sir:
We want to use INA234 on our application.
Do you have sample code for ARM or reference design?
Can you provide the link or document for us?
Looking forward your feedback.
Thanks…
Part Number: INA234 Hi expert,
Customer want to qualify INA234AIYBJR and require Halogen Free. Could you please clarify the statement in the DS if it can be considered as Halogen Free?
Regards,
Allan
Part Number: INA234 The INA234 returns the voltage, current, and power in the registers VBUS, CURRENT, and POWER. POWER is supposed to be the product of VBUS and CURRENT. Instead, POWER = 16 x VBUS x CURRENT.
Part Number: INA234 Hi Expert,
If INA234 is set as single shot mode and AVG is set as 111b=1024, will 1024 times conversion average be applied after trigger? Thanks.
BR,
Elec Cheng
Part Number: INA234 Hi team,
Is it possible to know whether we will have the power down mode in default version for INA234 device? Like INA231A and INA231B.
Best Regards,
Leroy Song
Part Number: INA234 Other Parts Discussed in Thread: INA219 , Hi,
We are using INA219 in our design . Due to long lead time, we would like to replace it with INA234. Could you please confirm if the functionality of both devices are same or if there are any…
Part Number: INA234 Hello,
I am having trouble with calculating the right power via INA234's power register (0x03). The datasheet provides the following equation:
Power [W] = 32 x CURRENT_LSB x POWER
If I were to use it, I would obtain enormous numbers…
Part Number: INA234 Hi team,
Why isn't least 4bit of POWER (3h) reserved? All shunt voltage (1h), bus voltage (2h) and current (4h) are reserved but only 3h is not reserved although 3h is calculated by those values. I think least 4bit of 3h should be…