Part Number: INA237 Hi,
according to the datasheet the INA237 has a config register in which you can set bit 15 (RST) to 1 in order to trigger a system reset.
Is it possible to set this bit to 1 and send all other bits of the config register in one i2c…
Part Number: INA237
Hi,
I am a bit confused about the INA237AIDGSR IC ground and load ground relationship...
The datasheet mentions "the common-mode input range and device supply voltage are independent of each other " and the following diagram denotes…
Part Number: INA237 Hi,
My customer faced this question, which is given following:
INA237 owns the VIL which is 0.4V, and the low-level threshold of the front-end chip output voltage is also about 0.4V. So that they are worried about the threshold and…
Part Number: INA237 Other Parts Discussed in Thread: SYSCONFIG HI,
We are getting different current readings from Ina 237. Each reading has a 150mA difference. If you have any sample program or sample calculation, please share it it with me.
1)circuit input…
Part Number: INA237 Other Parts Discussed in Thread: SYSCONFIG Hi expert,
Do we have Linux 5.4.164 driver for INA237 can share with customer?
Thanks,
Allan
Part Number: INA237-Q1 Other Parts Discussed in Thread: INA237 , I have a sensor loop reading the I2C data from eight INA237 shunt monitors every 100ms. The sensors are running in continuous conversion mode and I am reading them asynchronously. About 0…
Part Number: INA237-Q1 Hello Experts,
I have question regarding reading data from INA237-Q1. Is this chip supporting burst mode to read all the values in one transaction?
I've tried in several ways but always I was able to read only one registers.…
Part Number: INA237 Other Parts Discussed in Thread: INA740B Hi expert,
Customer want to use a power monitor at front of bridge diode for +/-57V in PoE application for example PR12-PR35 could be +57V or -57V.
Now we are considering INA237 or INA740B that…
Part Number: INA237 Hi Team,
In my application the output current might be zero and and I just want to use the overcurrent and overvoltage threshold.
Can I deactivate the undercurrent error on the ALERT pin in any way?
Will the alert pin trigger if I set…