Part Number: INA238 Tool/software: Hello expert,
May I know if INA238 could be used in AC input 90Vac~264Vac telemetry application? If AC is not acceptable, may I know if we can connect with certain circuit behind the full-bridge diode circuit? any…
Part Number: INA238 Tool/software: Hi Expert,
Do we have any Linux drivers released to the Linux community? The customer's switch project requires all drivers to be open source.
Regards, Hailiang
Part Number: INA238 Other Parts Discussed in Thread: PCA9306 , TCA9517
I’m getting a “no acknowledge” (NACK) when I try to communicate with the power monitor.
Part Number: INA238 Dear Sir/Madam,
I need help about INA238 power monitor IC. Suppose that IC ground reference name is GND. The supply voltage of INA238 is 5V.
I have another supply which has different ground reference and I try to monitor the…
Part Number: INA238 Other Parts Discussed in Thread: THVD8000 Tool/software: Hi,
I was testing out the EVK for the INA238 and I am using a 10mOhm shunt and planning to measure current between 0 to 3A with 1mA accuracy while minimizing the shunt resistance…
Part Number: INA238 Other Parts Discussed in Thread: INA228 , , SYSCONFIG Tool/software: Hi expert,
My customer ever used INA228 in some projects and they want to use INA238 in some cost-down project.
They want to know whether the software can be…
Part Number: INA238 We are using INA238 for current sensing, we are using Eval board INA238 with our ST microcontroller. We are using R shunt= 50 mOhm and it is calculated as per datasheet
For Shunt calculation referring this equation SHUNT_CAL = 819…
Part Number: INA238 Tool/software: Hello Team, We are using the voltage monitor INA238AIDGST for one of our applications.
The description of the ALERT pin is Open-drain alert output, default state is active low.
Does this mean the ALERT pin is low…
Part Number: INA238 Tool/software: for my aplication: maximum expected current= 90A, ADCRange=0,(163.84mV), Rshunt=0.001 Ohm This is my messure results up to 10A. It seems that as the current increases, the measurement error becomes larger.
is…