Part Number: INA238-Q1 Other Parts Discussed in Thread: INA238 Hi,
I have a set of boards where the INA238's A0 pin is connected to VS and the A1 pin is connected to SDA (address 1001001), but some of them ACK and send data at address 1001001 and others…
Part Number: INA238-Q1 Other Parts Discussed in Thread: INA238 We have a power distribution board with 40 power outputs. Each output can supply 3A, half of them are 28V the other half are 12V.
Example of one of the outputs:
So far we have produced…
Part Number: INA238-Q1 Other Parts Discussed in Thread: INA238 Hi I dont want to do any voltage measurement in my design using INA238, if VBUS pin is unused what should be the termination method for it, shall I leave it floating or connect to GND with…
Part Number: INA238-Q1 Other Parts Discussed in Thread: INA238 , ISO1540 , TCA9517-Q1
Tool/software:
Hi,
In addition to 4 temperature sensor devices communicating over the I2C bus, the PCB also includes an INA238 device.
During I2C communication…
Part Number: INA238-Q1 Tool/software: Hi Team,
Through current below link driver, we can measure mA current range, but we have a need to measure microampere range. So, what changes need to be done for measuring microampere current through current…
Part Number: INA238-Q1 Other Parts Discussed in Thread: INA238 Tool/software: We are using the INA238 current-sensing IC in a high-volume project. In our application, we need to completely disable the Alert signals via software without physically accessing…
Hello,
Divyaa M U said: 1.INA238 will work if powered with 3.3 Vs and 1.8V logic I2C interface?
Yes, the relevant datasheet specifications are pasted below. The INA238-Q1 only requires 2.7V on it's input and 1.2V for it's I2C logic, and these specifications…
Part Number: INA238-Q1 Other Parts Discussed in Thread: INA226 , INA238 Hi Teams,
Is the software of INA238 compatible with that of INA226?
I am planning to upgrade to INA238. How many software modification I need to do?
BRs,
Marsh