Part Number: INA239 Other Parts Discussed in Thread: SYSCONFIG , INA229 , TI-SCB , INA236 Hi!
Below is my simple setup using the INA239 on a device called the VCP Monitor 4 Click. I have provided the link to the device that the IC is built on, the schematic…
Part Number: INA239 The system routed "INA239" to the Amplifiers forum. Since it's actually a power (current/voltage) monitoring sensor, apologies if that's not correct forum.
The TI items are:
Sensor Control Board SENS077 Evaluation…
Part Number: INA239 Other Parts Discussed in Thread: SYSCONFIG
Hi,
I use INA239 to get VBUS and current.
I used Sysconfig.
Some rare case, I read 0x0000 on VBUS register.
The ADC is configured as continuous.
I read the register asynchronously.
Should…
Part Number: INA239 Hi Ti,
I have the slau839 controller, connected to an evaluation board ( SBOU241E ) with the INA239 installed.
I am able to measure and read the data out on he registers, but I don't get any data in the 'Results Data' Tab - the plots…
Part Number: INA239 Hello all, my goal is to design a very reliable PCB to test a product (motor). The INA239 measures the bus voltage (48V) and current (Imax 20A) going inside the motor. We are using an industrial power supply to simulate the battery…
Part Number: INA239 I wanted to make synchronous ADC measurements of only the shunt voltage with the INA239. For this i wanted to start the conversion in single-shot mode and use the ALERT pin as an indicator for a finished conversion.
My target timings…
Part Number: INA239 Hello all,
I would like to know more about the MEMSTAT bit in the DIAG_ALRT register. So far, the only information provided about it in the datasheet is (a) in Table 7-13 on page 27:
This bit is set to 0 if a checksum error is detected…
Part Number: INA239 Dear T.I. Experts, is it possible to write to more than 1 register while a ChipSelect=Low Period or must CS going high after every Reg.-Write? (Same for Reg.Read?)
Thanks in advance!
Part Number: INA239 Hi,
I want uo use INA239 to monitor the voltage and current, for get the detailed I/V curve need more sample point.
From INA239 datasheet, we only find the ADC conversion-time, and the MIN. A DC conversion-time is 50us, can we say the…
Part Number: INA239 Hello all,
When the current in my system exceeds what the datasheet calls the "maximum expected current" or "maximum current to be sensed" or "o vercurrent fault threshold" or "I max " I observe that…