Part Number: INA240 Hi All
Page 19 of IC datasheet gives an equation for Gain Error Factor = 3000 / (Rs +3000) where Rs is the external filter resistance value.
I would like some detailed insight into how the constant 3000 is calculated. Knowing…
Part Number: INA240 Tool/software: I am reaching out to request Coefficient of Thermal Expansion (CTE) data for the component. Could you please provide us with the CTE values ? We would appreciate it if you could provide the CTE values in ppm/°C or ppm…
Part Number: INA240 Tool/software: Hi ,
I am considering the INA240 series A1: 20V/V, A2: 50V/V, and A3: 100V/V.
Is it correct to understand that the circuit configuration of the above model numbers is only different in the resistors that determine…
Part Number: INA240 Other Parts Discussed in Thread: INA901-SP Tool/software: Hi,
Just wondering why INA240-SEP part is pulled out from TI? Is availability foreseen in the future?
BR,
MIka Hirvonen
Part Number: INA240-Q1 Tool/software: Does the reference divider accuracy (0.1% MAX) mean that the maximum imbalance between REF1 and REF2 is 0.1%?
For example, if Rref1 is 50 kΩ, does this mean that the resistance of Rref2 is between (1-0.1%)*50 kΩ…
Part Number: INA240 Other Parts Discussed in Thread: INA241A , INA296A Hi team,
Do we have a smaller package version of the INA240 and rated for 48V?
Thank you.
Kind regards,
Wouter Kragt
Part Number: INA240 Other Parts Discussed in Thread: INA181 Tool/software: Hello Team,
I wanted to have a accurate current measurement solution. Can i use INA240 as a low side current measurement on my battery gnd line(DC low side current measurement…
Part Number: INA240 Tool/software: I can't seem to find information on the gain of INA240PMPWTPSEP. Does anyone have this information? All datasheets link to the new version of the INA240.
Thanks!
Part Number: INA240 Tool/software: Hi folks,
We are in a need for a space qualified bi-direction current sense amplifier that’s compatible with a 3.3V or 5V power rail and has a wide common mode range?
Our current design has INA240PMPWPSEP, however…
Part Number: INA240-SEP Hi everyone, my point is the following.
I would know if the component can be used in a scenario where it is unsupplied (off), but a current flows in the shunt resistor
(so, a voltage in the order of tens/hundreds of millivolt…