Part Number: INA240-Q1 Dear TI Aerospace & Defense Team,
We are evaluating the INA240-Q1 as a replacement for the obsolete INA240-SEP in a Class D LEO spacecraft. Because the PCB has already been designed and qualified, a pin-compatible replacement…
Part Number: INA240-Q1 Other Parts Discussed in Thread: INA240 , INA149 What is the bias current in the INA240 when the differential voltage is very large—for example, 65 V or 80 V?
Will the device be damaged if it is held in this state continuously…
Part Number: INA240-Q1
Tool/software:
Hi team,
I need your help to recommend a P2P device with INA240-Q1(TSSOP package), but need higher slew rate and higher bandwidth.
Thanks!
Ethan Wen
Part Number: INA240-Q1 Tool/software: Hi Teams,
Is there any problem with the design of the INA240A2QDRQ1 chip to achieve ground fault detection for two ground wires?
Please help review the schematic diagram,
thanks.
The principle is that when…
Part Number: INA240-Q1 Dear Supplier,
Good day!
We are in the process of collecting information regarding the BMW DCDC Gen Basis Project
Kindly provide the details requested below, specifically the standard used for whisker testing and confirmation…
Part Number: INA240-Q1 Tool/software: Does the reference divider accuracy (0.1% MAX) mean that the maximum imbalance between REF1 and REF2 is 0.1%?
For example, if Rref1 is 50 kΩ, does this mean that the resistance of Rref2 is between (1-0.1%)*50 kΩ…
Part Number: INA240-Q1
Hi Team,
We had previously requested the PPAP and data information for this INA240A2EDRQ1. We have now received the PPAP for the part, and thank you for providing that.
At this stage, we kindly request you to provide the…
Part Number: INA240-Q1 Other Parts Discussed in Thread: INA901-SP Tool/software: Hello,
Can you provide information on the packaging material for part number INA240-Q1 (specifically ordering P/N INA240A1QPWRQ1)? Our intent is to use this in a vacuum…