Part Number: INA241A Other Parts Discussed in Thread: OPA388 , Tool/software: Dear Supporter:
We are trying to use this chip to sample current (range +/- 100A ) in high side with ~5V common voltage.
However we are not able do frequency compensation…
Part Number: INA241A Tool/software: Servo_Driver.pdf
We designed servo driver based on DRV8256E. We have shunt resistor that measures the current and use INA241 to amplify the voltage across the shunt.
In the two pictures we can see waveforms of…
Part Number: INA241A
Tool/software:
Hello, we use the INA241A-Q1 as an in-line shunt amplifiers for a 48V motor drive application.
When a motor phase goes high-to-low, or low-to-high, the common-mode voltage across the shunt change would cause…
Part Number: INA241A Other Parts Discussed in Thread: TIDA-010936 Tool/software: Hello, I am interested in using your INA241 IC in inverters with a switching frequency of around 100 kHz.
You have a GaN inverter demonstration board (TIDA-010936). Could…
Part Number: INA241A Tool/software: Hi Expert,
my customer wants to use INA241 x 2 in motor drive phase current sensing, is there one chip solution for 2 channels INA241?
Or other small size solution to replace INA241x2
Thanks
Eason
Part Number: INA241A Other Parts Discussed in Thread: TL072 Tool/software: The test data shows that the gain error is very large, beyond the accuracy of the gain error given by the chip, help to see what is the reason
Part Number: INA241A-Q1 Tool/software: Hi all.
I'm using INA241A3-Q1 shunt amplifier. I have some problem. We got boards from assembly. During testing one of INA241A3-Q1 has burnt:
I'm trying to understand what could be a cause of it.
I…
Part Number: INA241A Tool/software: Hi Team,
Do we have any other devices which have higher common mode voltage stress? Customer increase output voltage from 54V to 400V. Thanks in advance.
BRs,
Francis
Part Number: INA241A Tool/software: Hello,
We are planning on selecting the INA241A2 with a 5ohm shunt to sense the current on the 3 phases output of our GAN inverter.
The current level is 4A mean / 8A peak per phase.
We intend to run our PWM at…