Part Number: INA271 Hello guys,
One of our customers is evaluating INA271 now. Their evaluation circuit is almost same as the simplified schematic on page 1 in the device datasheet (SBOS381E). But one point is different from the schematic. it is that…
Part Number: INA271 Other Parts Discussed in Thread: INA282 , INA240 , LMP8645HV , Hi Team,
Do we have a pin-to-pin device with the INA271AIDR that has a higher gain, closer to 40V/V instead of 20V/V?
Thank you,
Jared
Part Number: INA271 Hello,
I used five INA271 circuits with 20 mOhm shunts on my board to sense current on five different voltage rails.
Two of the INA271 circuits are working fine. Three of them however, are not. Their are experiencing variable gain…
Part Number: INA271 Other Parts Discussed in Thread: INA282 Hi,
Am using INA271 Current sensing amplifier in by dual phase synchronous buck design ..My shunt resistor value is 2 milli ohms ..
am getting different output voltages corresponds to the input…
Part Number: PGA305EVM-034 Dear, support team.
I have questions in circuitry around OWI in EVM.
No.1
This is OWI Block Diagram in datasheet (PGA305 EVM).
What are the functions of Offset Voltage and Current Compensating Voltage.
Is the circuit required…
Other Parts Discussed in Thread: INA271 Hi team,
My customer Innovation is evaluating our INA271AQDRQ1 in their EPS system for current sensing. When doing output error vs common mode voltage test (with 5V supply), customer first tie Pin1 and Pin8 togather…
Part Number: LMP8601 Other Parts Discussed in Thread: INA271 ,
Hello,
I'm using following circuit for bidirectional current monitoring using LMP8601-Q1.
I have some design requirements of measuring +/- 15V with maximum of 2A flowing through it. Initially…
Hello Stefan,
Thank you for your question and using the E2E forum.
Current sense catalog can be searched and filtered here(can filter by package and sort by CMRR):
Current sense amplifiers product selection | TI.com
That being said INA270/271 is only…
Leonard, Artzy,
As intuitive as it seems given the 24V common mode here, current sense amplifiers are typically not used in 4-20mA applications because of the size of the shunt resistors typically utilized for these systems against the increased nature…