Part Number: INA280 Hi
Could you offer some advice?
The customer plans to replace the current part LTC6101HVAIS5, and has found the TI INA280A2 themselves.
Part Number: INA280-Q1 I see in the INA280x-Q1 datasheet that the maximum recommended load capacitance is 500pF without an isolation resistor. Is there any guidance on sizing the isolation resistor in order to support a larger output capacitance?
My…
Part Number: INA280 Tool/software: The P-Spice model for INA280A1 does not work as expected. It seems that Vss and GND pins are swapped. Also, the output voltage does not change with input changing.
Part Number: INA280 Other Parts Discussed in Thread: OPA192 Tool/software: Hi
The customer is using INA280A4 for output current detection, and the application circuit is the same as the typical circuit on the first page of the datasheet. However, at…
Part Number: INA280-Q1 Other Parts Discussed in Thread: INA280INA280-Q1 Failure mode
Vdiff= 0V, but Vout=5V , What failure of INA280 can cause such a phenomenon ?
note: VIN+ and VIN- not exceeding the specification
Part Number: INA280 Tool/software: It looks that the current operation is only for unidirectional for INA280/x290. Is there bi-directional operation with 120V,max derating?
Regards
Brian
Part Number: INA280-Q1 Other Parts Discussed in Thread: INA280 , INA290 , INA200 , INA381-Q1 , INA301-Q1 , INA300-Q1 Hi Team,
Our customer would like to know the minimum Vsense that the INA280-Q1 can amplify.
Regards,
Danilo
Part Number: INA280-Q1 Tool/software: Hello,
i have a INA280-Q1 that is supply with 5V that i use to measure current through a shunt connected to Vcm = 9V. In my application Vcm can be switched off.
According to the datasheet this should not damage…