Other Parts Discussed in Thread: INA282-Q1 Dear Support Team
Could you provide data of Swing to V+ Power-Supply Rail in 6P of datasheet at below condition?
◆Condition Device:INA282-Q1 Ta:-40~125℃ Output current:0.2~20uA
Regards
Tomohiro Nagasawa
Hi,
The reason we didn't include these 2 applications is because we are planning to update the application with some more information in a separate application note. As of now we do not have a firm date as to when this will be released but hopefully sometime…
Ella,
For possible pin to pin replacements for the SOIC version of the device (D), I would recommend looking at the automotive version, the INA282-Q1, as well as the INA240.
Note that the INA240 is not functionally equivalent, and the customer would need…
Other Parts Discussed in Thread: INA282-Q1 I would like to confirm impulse noise of INA282-Q1.
The customer wants the pass of the test ;
Pulse cycle: 10ms, Pulse width: 1us, Test period: 10 minutes, Test voltage +/- 500V (must), +/- 2kV.
If you have the…
Part Number: INA286 Other Parts Discussed in Thread: INA282 , INA293
Hi, Support Team
1. The load is an electronic load with CC mode and we have also applied a CV on Shunt-Resistor to generate a DC current (all PWMs and Power Stage are stop), the output…
Part Number: INA190-Q1 Other Parts Discussed in Thread: INA190 , INA240 , INA293 , INA282 Dear TI Experts,
i am planning to replace INA240A2-Q1 with INA190A2-Q1 due to supply chain/availability constarints.
at present, as i have shown CSA is in LOW SIDE shunt…
Oddly LM4041 CIM3 has 45µA minimum operating current, was out of tolerance with 6K8, roughly 40µA . R166 3K9 gives +5V / 3v3 LDO switching noise isolation and 85.6µA minimum operating current. Older schematics only show R166=10k so it was never…
Other Parts Discussed in Thread: INA282-Q1 , LMP8602 , INA282 Hello everyone,
I am facing a problem for which I can't seem to find a solution.
I need to measure a current through a shunt resistor and current sensor amplifier, for which "standard" components…
Part Number: INA240-Q1 Other Parts Discussed in Thread: INA240 , INA282 Hi team,
We are considering using INA240 as shown in the following figure.
Could you tell me the resistance value in red?
In our usage, current flows in from IN +, and the REF2 and…