Part Number: INA293-Q1 Other Parts Discussed in Thread: INA293 , INA190 , INA186 Hi all,
I use INA293 to measure low current (10uA) with high voltage (max 100V).
Without load I see 40uA of consumption from the power supply and also some mV on the output…
Part Number: INA293-Q1 Other Parts Discussed in Thread: INA240 Hi team,
INA293-Q1 is a uni-Directional device.
May I know how to configure INA293-Q1 to Bi-Directional Circuit by adding some biased voltage or REF? Like INA240 intenal block.
Thanks!
Part Number: INA293-Q1 Hi,
in the datasheet the status is listed as active. However on your Website it is listed as preproduction. I would appreciate info on which of these two true, and if possible info on when the device will be available.
regards…
Part Number: INA293-Q1 Other Parts Discussed in Thread: INA195 , INA293 Hi,
I intend to use INA293A3QDBVRQ1.
I want to ask a question:
Now I’m using INA195 and in the datasheet the gain error is declared 20mV<
I want to use INA293 but I can’t tell…
Part Number: INA293-Q1 Other Parts Discussed in Thread: INA193 , INA293 What is the current sinking and sourcing capability of the INA293-Q1? I couldn't find it in the datasheet.
Part Number: INA196A-Q1 Other Parts Discussed in Thread: INA196 , INA290 , INA280 , INA240 , INA293 Tool/software: Hi,
Good morning.
What happens when we connect one end of 1 Ohm resistor to pin no 1 of INA196AIDBVT and the other end of the resistor to the…
Hey Shinichi,
Since this behavior is not tightly controlled there is no specification. However, based upon testing we have done, it seems like the overload recovery delay may only last up to 80 µs assuming a -70mV input. I would say that you would need…
Hi Devendhiran,
To address your questions point-by-point:
1. It is not advisable to place a 1k resistor in series with the input pins, a maximum of 10 ohms is allowed.
2. When you place a large input resistance in series with your input pins; (i) there…
Hey Harry,
The only way to improve this for INA214 is to provide a small reference voltage to REF pin (> 50mV). This will ensure OUT is always in linear region.
The other option is to simply use a faster device such as INA181, INA280, or INA281. The…
Part Number: INA290-Q1 Other Parts Discussed in Thread: INA290 , INA293 , INA190 Hi,
We would like to use low side current measurement with INA290. I see many high side current measurement applications on datasheet but is there any problem about low side…