Part Number: INA300 Tool/software: Hello, I am trying to simulate INA300 in Simetrix using INA300 Spice model downloaded from TI. Simulation runs 15us only and then has no convergence in transient analysis. I tried different integration methods (Trapezoidal…
Part Number: INA300EVM Tool/software: Hi Sir,
I am trying to measure CMR and PSR, could you teach me how to measure this spec?
becasue this is comparator, I am not sure could I measure it same as OP, VOUT measure point is /ALERT? VIN is IN+/IN…
Part Number: INA300 Dear TI Teams,
One of our new project need to use a 65W adapter (20V/3.25A). We to detect the signal of the adapter, when the adapter is detected to be inserted, EC will enable INA300 to achieve real-time monitoring of the pressure…
Part Number: INA300-Q1 Other Parts Discussed in Thread: INA300 Hi team,
I have some questions here.
1. My customer is using INA300 for BCM application but based on cost they don't want to add bidirectional operation . I would like to know that what…
Part Number: INA300-Q1 Hi team,
In customer's system, the common mode input voltgae can be -0.2V ~ -0.1V. This doesn't exceed the abs max voltage, but this exceeds the electraical characteritics, that is 0V.
What can we mention about this? The understanding…
Part Number: INA300-Q1 Other Parts Discussed in Thread: INA300 Hi Team,
I'm utilizing the INA300-Q1 in my design for overcurrent protection, and the schematic is provided for your reference.
The design is intended for two different loads:
1. 12V…
Part Number: INA300 Other Parts Discussed in Thread: INA301 , Hi,
We have an INA300AIDSQ designed in to our device. However, these turns out to be hard to find, so to enable production quicker we are looking into changing to a INA301 since that is available…
Part Number: INA300 Hi I would like to use INA300 in a design for overcurrent protection. Section 7.3.1 of the datasheet talks about the sense resistor voltage can be monitored for a sense resistor drop of up to 250mV. I have a current monitor level set…
Part Number: INA300 Hello,
I am currently using the INA300 for over current detection. The limit resistor is set to 836 ohms and the sense resistor is 0.291 ohms. The hysteresis pin is floating so the hysteresis value should be 2 mV.
Given his information…
Part Number: INA300 Hi team,
Customer consider use INA300 in their project, and they get one question about the Alert status during disable state.
They plan to let the part work in LATCH mode, when the ALERT signal get latched, and if they disable…