Part Number: INA303-Q1 Please confirm the following calculations: - A Pull Low Signal is triggered when the actual charging current is 20A. - A Pull Low Signal is triggered when the actual discharging current is 30A. - A 100kohm pull-down resistor on…
Part Number: INA303-Q1 Other Parts Discussed in Thread: INA303 Tool/software: Dear Texas Instruments Support Team,
I am using the INA303 as a window comparator in a BMS application to monitor current sensing and short-circuit detection.
We are facing…
Part Number: INA303-Q1 Tool/software: Hi Expert,
Regarding to the delay function of second comparator, I don't quite follow how delay work.
For example, the delay time is set to 2ms, Vlimit2 is about 3.5V. If there have a 4V/1.5ms voltage pulse on…
Part Number: INA303-Q1 Hi Experts,
The alert pin of INA303-Q1 is active low, customer want active high, can they set lower threshold of ALERT1 than ALERT2? See pictures below, INA303-Q1 is configured in bi-directional monitoring mode. Customer want…
Part Number: INA303-Q1 Hello team,
I am Oliver Kim who supports automotive customers in TI Korea.
Could you share the INA303-Q1 sample and RTM schedule? Can I get the samples by the end of April?
INA303A1QPWRQ1
INA303A2QPWRQ1
INA303A3QPWRQ1…
Part Number: INA303-Q1 Other Parts Discussed in Thread: INA303 Hi,
I am trying to simulate INA303-Q1 for my application. The maximum input that can come across the positive and negative input of internal OPAMP is 33V continuous input.
When I simulated…
Part Number: INA303-Q1 The integrated current sense amp+dual comparator IC features one of the comparators' output delayed (comparator 2: Latch 2 and Alert 2).
Section 7.3.3 of the datasheet has the delay calculation formula in the attached snipet.…
Part Number: INA303-Q1 Hi TI Team,
We have considered INA303A1 current sense amplifier for our design.
We are using this device for bi-directional current sensing.
So we have given an external 2.25 V REF reference using a simple voltage directly…
Part Number: INA303-Q1 Other Parts Discussed in Thread: INA303 , DRV8313 , INA302 , INA301 , TIDA-00778 Hi there,
Right now I´m building a custom PCB for a motor controller that will use FOC. The driver/h-bridge that I use is DRV8313 and it needs additional…