Part Number: INA381 Tool/software: Hello,
I am designing a single cell charger and I have used INA381 to detect when the output consumes more than 50mA of current. Could you review the design I made regarding INA381A4 and comment if it is ok, or if…
Part Number: INA381-Q1 Hello TI support team,
In the following thread the digital input leakage current of the INA381-Q1 was discussed: INA381-Q1: Leakage current of Digital inputs over full operating temperature range - Amplifiers for…
We've used…
Part Number: INA381 Other Parts Discussed in Thread: INA303 , INA302 , INA300 1m ohm shunt is used to measure current. 2 INA381 ICs are used to measure bidirectional current in battery for charge (6A) and discharge (110A). When ever Surge is applied across…
Part Number: INA381 Hi TI Teams,
From the datasheet of INA381, we know that its available gain is INA381A1(20V/V), INA381A2(50V/V), INA381A3(100V/V) and INA381A4(200V/V). Now the maximum current used in our project is a little more than 2A, how should…
Part Number: INA381 Tool/software: Hi Team,
My customer is now evaluating INA381 for their application and some questions may need your confirmation, thanks.:
1. Is it the logic high & low threshold for RESET pin as well?
2.Do we have accuracy…
Part Number: INA381-Q1 Tool/software: Dear TI experts,
My customer drew their schematic using INA381-Q1. Could you review this schematic?
They just want to VOUT high if HEATER_CONTROL is high. And B+ is 12V of car battery.
Please let me know if…
Part Number: INA381-Q1 Other Parts Discussed in Thread: INA381 Tool/software: Hi Team,
Customer wants to know the total power consumption of INA381. There is no information in the datasheet. So please check it and let me know.
Regards,
Part Number: INA381 Other Parts Discussed in Thread: TLV9152 , , LM2903 , INA180 , TLV3231 Tool/software: Hi team,
I'm looking for op amps and comparators that enable high-speed overcurrent detection for compressor motor. Could you tell me the fastest…
Part Number: INA381-Q1 Tool/software: Hello TI,
I am looking for some information regarding the internal comparator of INA381-Q1. It's good that the "High-level input voltage", "Low-level input voltage" and "Alert low-level output voltage" are specified…