Part Number: INA381-Q1 Other Parts Discussed in Thread: UCC27424 Hello TI,
I am currently simulating the behaviour of INA381-Q1 during over current condition as shown in the below circuit. I have created an over current situation by placing a low resistance…
Part Number: INA381-Q1 Hello,
1) Please specify the maximum leakage current for CMPREF pin considering junction temperature up to 125 °C.
2) Please specify the maximum leakage current into CMPIN pin when the hysteresis current source is not active…
Part Number: INA381-Q1 Other Parts Discussed in Thread: INA381 Hi Team,
According to the customer's RI test result, there was a failure at 1200MHz to 1400MHz due to the fluctuation of current sensing value. [1200MHz to 1400MHz, PM(PRR=300Hz, PD=3us…
Part Number: INA381-Q1 Other Parts Discussed in Thread: INA381 , UCC27524 , UCC27444 Hi,
The customer questions the INA381 simulation results.
The result is that when INA381A4 recognizes overcurrent, the Alert output is in Latch Mode, but it operates…
Part Number: INA381-Q1 Other Parts Discussed in Thread: TINA-TI Dear All,
What is the INA381-Q1 behavior when the reverse current scenario (VIN- > VIN+)?
Especially, the VOUT and ALTER status.
Regards,
Dylan
Part Number: INA381-Q1 Hello,
I received INA381A2QDGSRQ1 marked as 22P7 but the datasheet only shows 22P6 as the identifying markings. Are these parts incorrect or is 22P7 another valid marking?
Thanks for the help,
-Kyle
Part Number: INA381-Q1 Dear TI,
Kindly provide the Safety manual and detailed FMEDA for the iNA381-Q1 (A1 version) device for the functional safety assessment.
Let me know if any clarifications are required.
Regards,
Anand M
Part Number: INA381-Q1 Hi,Team,
Though my customer knows that the sink current of ALERT pin is limited by a pull-up resister, They would like to know the maximum rating current of ALERT pin.
Please tell me the absolute max rating for DC and Peak current…
Part Number: INA381-Q1 I have a question related to the input impedance in the following E2E post.
https://e2e.ti.com/support/amplifiers/f/14/p/917744/3391574#3391574
In electrical characteristic table on INA381-Q1 datasheet, there is the specifications…