Part Number: INA4180 Other Parts Discussed in Thread: INA4181 , INA185 low side shunt current sense circuit is designed as shown as below,
design spec: low side shunt current sense/ gain=37/ max frequency=30kHz/ as less 3 output in one package/ Vin…
Part Number: C2000WARE-MOTORCONTROL-SDK Other Parts Discussed in Thread: MOTORWARE , INA4181 Hello,
We are following up on this thread: https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1055503…
Hi,
The INA240 will be suitable at this frequency. You will need to evaluate if it can settle fast enough if duty cycle can go to extremes.
We currently don’t have an inline current sense amplifier (CSA) equivalent that is cheaper.
If you use low…
Max,
Unfortunately, we do not offer 4 channel digital power monitors. But we do have 4 channel analog monitors available if your customer decides to go that route.
The 4 channel analog monitors offered are:
-INA4180-Q1
-INA4181-Q1
-INA4181…
Hello SHH,
As the PAC1934 is a quad digital power monitor, our cross options are pretty limited. Our only multi-channel device of this type is the 3-channel INA3221. Unfortunately the INA3221 does not offer the power accumulator function of the PAC1934…
Part Number: INA4180 Other Parts Discussed in Thread: INA180 , INA240 Hi Team,
Would it be okay to use a 100kohm resister and 100nF capacitor at the input for low drive application. I read that for high side we can't use resistor greater than 10ohms…