Part Number: INA592INA592 is used for Voltage to Current conveter. My circuit expected to work as
i. Sink mode Configuration: Vin below 1.25V current(0-20mA) should flow and if Vin above 1.25V then 0mA should flow.
above is working fine if My INA592…
Part Number: INA592 We are using INA592(Gain=2) as Loop monitor with 1.25V offset. i am getting same voltage output i.e 1.3V (at ADC_in) when loop is 1mA flowing in the loop but i am expecting 1.25V when it is floating.
i am attaching two simulation…
Part Number: INA592 Other Parts Discussed in Thread: OPA2196 , TMUX6219 , OPA310
We have recently designed a V-to-I converter for our 3-wire transmitter using the INA592, OPA2196, and TMUX6219.
We are observing a back-powering issue when the loop…
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: AMC3301 , INA592 I am able to get the TINA model for the AMC3301 + INA592 working.
With PSpice for TI , I can get the individual components (AMC3301 and INA592) to work.
However, with PSpice…
Part Number: INA592
Tool/software:
Hello,
I'm working on modifying a 9V battery-powered handheld DC current source that needs to be able to source +1nA-500uA with <1% error. Temperature range is from 65-75 degF (18-24 degC). The circuit is similar…
Part Number: INA592 Tool/software: I built the following circuit using INA592. The voltage measured across R164 doesn't match my expected value. Theoretically it should be (V / R147) * R164. Where could the issue lie?
Additionally, I measured the voltage…
Part Number: INA592 Tool/software: Hello Team,
Posting on behalf of customer:
Our device INA592IDRCR has an MSL1 rating, but the reel arrived in a moisture barrier bag and shows MSL2 - is it common for our devices to arrive in a higher rated MSL bag…
Part Number: INA592 Other Parts Discussed in Thread: INA597 , STRIKE Tool/software: I'm trying to use this part in the G=2 mode, datasheet states this is possible. I have the -IN connected to OUT and the source negative input goes to SENSE, and the source…
Part Number: INA592 Other Parts Discussed in Thread: XTR305 Tool/software:
Fig1: Current Source Circuit
Fig2: Current Sink Circuit
Current Source Circuit (Source Mode): The circuit generates a current of 4-20mA when V2 is varied between…
Part Number: INA592 Other Parts Discussed in Thread: OPA593 Dear members,
I need to make a part of my design to be a HOWLAND PUMP for driving up to 100mA. Doing the simulations I could have maximum 60mA of load. I know that the MAx output current…