Part Number: INA823INA823_non_linear_behavior.TSC
Firstly i admit i may have missed something in the data sheet but.....
supply voltage 3.3
input common mode voltage = 1v
Vref =0v
Rg=20K => Av=6
differential signal ramp from 0 --> 0.4v
Problem…
We started to use the differential nature of the 1220 but ran into protection leakage issues. Added the INA823 in front with its 60V protection and set its reference to half our 4.096 ADC reference.
Based on your comment we are going to insert 2.048 (from…
Part Number: INA828 Other Parts Discussed in Thread: INA823 ➀ Temperature specification compensation of 125°C or more and low temperature drift ② it is possible from a common-mode input range of 0V with a single supply (assuming +5V) vs an output, and…
Part Number: ADS1120 Other Parts Discussed in Thread: INA823 Below circuit used for reading the mV input voltage from sensor with excitation voltage of 10V. Need some technical review is this circuit meet our expectation.
kindly review and let me your…
Part Number: INA333 Other Parts Discussed in Thread: INA133 , INA630 , INA826 , INA823
Hi Team,
My customer mentioned when powered up the device looks latch-up and then the device would be broken.
Could you check the schematic?
high side sensing: common…
The example values in this circuit result in a gain of 1. Is this not what you want?
There are integrated difference amplifiers like the INA154/INA132/INA152 or instrumentation amplifiers like the INA823/INA826/INA188 with more accurate resistors.
Part Number: XTR117 Other Parts Discussed in Thread: INA321 , LM317 , INA823 , XTR115 , XTR116 , XTR111
0081.pdf
Dear Team
I have designed the 4-20mA transmitter using XTR117(transmitter) and INA321(amplifier)
I am facing issues in this particular design…
Hi Jan,
In addition to Clemens suggestion, you may also try INA823 as shown in the image below.
Jan Croes said: has a bandwidth over of 4kHz
If this is the hard requirements at gain of 1000 V/V, then you may have to pick higher BW instrumentation amplifier…