Part Number: IWR1443BOOST Other Parts Discussed in Thread: INA826EVM , , DCA1000EVM , IWR1443 , INA826
I have a IWR1443BOOST connected DCA1000EVM and I am using a INA826EVM as external trigger. The INA826EVM is connected to a USRP N210 and being powered with…
Nicolas
You are correct, this is an error in the data sheet. Figure 73 is incorrect; all of the other figures are correct.
I will notify the document team and get this updated.
For an example of a suggested layout you can use the INA826EVM. I would be…
Part Number: INA826 Hello All,
I am using INA826AIDRGR in SON package with thermal pad. The part is connected as Wheatstone bridge load cell amplifier. Circuit diagram is exactly like recommended in INA826EVM,
Gain is set to 1000 with 49.9 Ohm across…
Part Number: IWR1443BOOST Other Parts Discussed in Thread: INA826EVM
I have an IWR1443BOOST board connected to a DCA100EVM using the 60-Pin adapter. I have modified the DataCaptureDemo_xWR.lua file to continously transmit and receive data. I ran the…
Other Parts Discussed in Thread: INA826EVM , OPA333 Hello,
sorry for my English it is not my first language.
I am new to electronics.
I have a problem regarding INA826EVM.
I am trying to build a circuit on the INA826EVM board (see attachment for a schematic…
Dear Wei,
Thank you very much for the quick and thorough response. Fyi, the input current on my INA826EVM (ordered 1 month ago) is only 1 to 1.2mA @ +/-15V, 25 deg C, at power-off. So it is way off the typical 6.5mA value. Maybe a recent change to the…