Part Number: INA826 Hello,
The datasheet states in the Characteristics table, that the Output offset is referred to input (RTI). so for the output offset, I would multiply the 200uV with the selected gain.
but in the formula, that is referenced by the…
Part Number: INA826 There is a schematic diagram in which the +vs =24V ,-VS=Ref=0v, +IN < 24v , +IN > -IN >0v and G=1 as following:
Question: Is the equation true ?
Vout = G*(IN+ - IN- )
Thanks,
John
Part Number: INA826 Other Parts Discussed in Thread: TPS2661 , In this app note: https://www.ti.com/lit/an/sbaa551/sbaa551.pdf what is the purpose of R1 and R9 on page 3. Also what type of capacitor would be best for this application (such as C4)? I was…
The output noise scales with gain BUT 20nV/rt-Hz and 21nV/rt-Hz noise spectral density refer to the input and NOT the output noise - see below. Vout_noise_rms=Vnoise*sq-rt(BWn)*Gain where Vnoise is the input noise spectral density and BWn is the noise…
Part Number: INA826 Other Parts Discussed in Thread: INA821 , INA819 Hi Team,
Could you pls recommend a device to replace AD8226BRMZ-R7 with 0.1% Gain error @ G = 5 to 1000? Thanks
Regards,
Hailiang
Part Number: INA826 Hi Amplifier team,
CMRR is ratio of differential gain and common mode gain. The datasheet says that it is referred to the input. What does referred to input mean here?
Regards,
Shaury
Part Number: INA826 Hi experts
In the ordering information for this device the INA826AIDGK lists the carrier type as BULK with quantity = 80. Can someone explain what that means?
Are they just loose in a bag? Is it tube?
Thanks!
Jim B