Part Number: INA827 I have two questions about the INA827 and two pieces of information for TI related to apparent errors on the part's data sheet (SBOS631B-JUNE 2012-REVISED NOVEMBER 2017).
1st Question:
I am interested in uses of this part immediately…
Part Number: INA821 Other Parts Discussed in Thread: INA819 , INA826 , INA827
Tool/software:
Hi experts,
I am looking for an in-amp that meets the following specifications. I checked TI.com and found that INA821 and INA819 looked good. What are the benefits…
Part Number: INA827 I am attempting to use this instrumentation amplifier to amplify a DC signal that ranges from 0V to 114mV. This range does not give enough resolution for my data logger system. I built the circuit according to the typical application…
Part Number: INA827 Other Parts Discussed in Thread: REF3425 , , OPA330 , REF3225 , INA821 , OPA320 , REF5025 I am considering using the REF3425 voltage reference to bias the output of the INA827 instrumentation amplifier by 2.5V. I have two questions:
The…
Part Number: TMUX1209 Other Parts Discussed in Thread: INA827 , ADS1261 , , TMUX1109 Tool/software: Hi,
I have designed a schematic for an analog measurement as shown below. On the analog input side, I can also receive negative analog signals from some…
Part Number: INA827 Rg= 80ohm, Vpower=8V.
Without any input signal (Granded for both -IN, +IN) there is almost 22mVpp on output.
No appearently noise on Vdd.
What kind of things I have to concern to reduce more output noise.
BEST REGARDS,
Hironari
Part Number: INA827 Hi,
We are using the INA827 instrumentation amplifier as the first stage in an IF circuit to convert a differential signal to a single ended signal. For biasing we have a resistor connected between each of the input lines and a Vcc…
Part Number: INA827
What is the tolerance of the internal 8k, 10k, and 50k resistors?
Most parts measure, the sum, 68k about perfectly. At least within 5%.
Some parts measure about 75k ohms or more