Part Number: INA849 Other Parts Discussed in Thread: INA848 , Hi,
What is the approximate output voltage swing under 2kΩ load, 70°C and ±14V supply? I need to output a signal of about ±12.5V, the datasheet only has value of 10kΩ load, 25°C, ±15V supply…
Part Number: INA851 Other Parts Discussed in Thread: INA848 Tool/software: Hi,
I'm using INA851 to drive a small signal to multiple instrumentation amplifiers for a calibration path,
the INA851 is feeding in parallel multiple instrumentation amplifiers…
Part Number: INA101 Other Parts Discussed in Thread: INA149 , INA848 , RES60A-Q1 Tool/software: I want to design a current amplifier for measuring current through motors buy using shunts
the motors are DC
AC 3 phase motor
AC Pwm motors
frequency…
Hello Sizhou,
The schematic makes sense to me, here are my comments regarding the gain settings. Please correct me if I am misunderstanding.
Internal Vexc is set to be 1.3V from the internal reference of 2.5V. The minimum offset from the sensor is…
Part Number: INA849 Other Parts Discussed in Thread: INA848 , , INAEVM-ALT-SO8 I have selected an INA848 IC instrumentation amplifier for a project for the following unique features observed in it’s datasheet that matches my requirement. - Output Amplitude…
Part Number: INA849 Other Parts Discussed in Thread: INA848 Hello,
I have a current source driving a laser diode. I would like to measure the AC component of the drive current so that I can characterize the source's noise.
I plan to use the INA849…
OK. So the INA849 comes in 2 versions: SOIC-8 and VSSOP-8. Are there any evaluation boards for the VSSOP-8 version? I guess not. :-)
I just discovered a variant with a fixed gain of 2000: INA848. It has CMRR = 132, whereas INA849 has CMRR = 120. But…
Part Number: INA826 Other Parts Discussed in Thread: LM358 , ADS1299 , INA851 , INA848 HI,
When we applied the INA826, we found that there is a certain DC component in the input differential mode signal.
Please send us the reference design or information…
Part Number: INA333 Other Parts Discussed in Thread: LM4120 , INA848 , INA818 , ADS1115 Hi team! I'm working on an amplifier for strain gauges, it will work with 120ohm strain gauges @5V. Based on this circuit , an ina333 is used to amplify the unbalanced…