Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: AM2434 Tool/software: Hi Expert,
I am looking for clarification on which SDK to use for a new project that is based on an existing codebase which used an older TI MCU-PLUS-SDK (v8.05).
The only industrial comms feature previously used was…
Part Number: MCU-PLUS-SDK-AM243X Tool/software: I use the AM243X Industrial COMMS SDK 09.02.00.09 and I found the LwIP interface source code for ICSS-EMAC doesn't support concatenated pbuf.
In the file am243x-mcu-plus-sdk\source\networking\icss_emac…
Hi Andrea, Issac,
You can work with just Industrial Comms SDK, now to add IPC project to CCS along with CCS:
1. Import Ethercat project into CCS- This you have already done
2. Import IPC project from the location: ind_comms_sdk_am263x_09_00_00_04\mcu_plus_sdk…
Part Number: TMDS64EVM Tool/software: Hi,
I am testing ipc_rpmsg_echo_linux example on TMDS64EVM.
When I started and stopped r5 core repeatedly, system hanged or linux panicked often.
log1:
root@am64xx-evm:~# head /sys/class/remoteproc/remoteproc[0…
Hi Archit,
Thank you for your reply.
I understood that it will be fixed in Industrial Comms SDK v9.2.
We are looking forward to the release of Industrial Comms SDK v9.2.
Hi Stephen,
Stephen S said: may I know where I can find the interrupt priority levels of other peripherals? as far as i Know, IPC comms also utilize interrupts, may i know priority level of IPC comms?
You can set the priority level of peripheral while…
So as far as I can tell from a header file (osdvr_version.h) it looks to be IND SDK 1.1.3.3. The ECAT firmware version, I am unsure what it was before (is there a way to tell?). The master stack we are using is made by Acontis. We also tested with an ackermann…
Hi,
gear c said: However, the kernel image built by myself is too slow.
How about the pre-built images that are provided as part of the SDK? Have you tried with that? Are they slow as well?
[ 15.312085] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up…
Hi Joshua, The Industrial Comms SDK v9.2 is available on ti.com at this link : https://www.ti.com/tool/download/INDUSTRIAL-COMMUNICATIONS-SDK-AM243X Regards Archit Dev