Hi Tanmay,
I thought of using bit18 of register 0x0FA00024 of sd to detect it, but the kernel crashes while reading the register.
I added a piece of code to the kernel source code ti-processor-sdk-linux-adas-j722s-evm-10_00_00_08/board-support/ti-linux…
What combinations DO NOT work?
EtherCAT Ethernet ports with a OPCUA port
2 Industrial Ports (MII): PRU_ICSSG1
1 OPCUA Port (RMII): CPSW
Pinmux Conflict
The ICSSG1 MDIO only has the option of using "PRG1_MDIO0_MDC" and "PRG1_MDIO0_MDIO"…
Hi Fabiana,
The error log shared is not build time error but its runtime error of onnxrt_ep.py , I have attached the error .
onnxrt_ep_error_log.txt
root@j721e-evm:~/edgeai-tidl-tools-10_00_05_00/examples/osrt_python/ort# python3 onnxrt_ep_dock107_blockage_fncwc_int8…
Hi Teja,
Thanks for your information.
I am trying to test the enet_lwip_icssg_am64x-evm_r5fss0-0_freertos_ti-arm-clang in industrial SDK v9.02.
However, error occord when import CCS project to CCS v12.6.
I done Re-install SDK, re-boot my PC, installing…
Daolin - my application does require RT-Linux; and I am using the A53s for those high speed comm paths.
It is interesting that the " tirex" path lists Industrial Communications SDK for AM64x for the description without stating it's for RTOS only…
Hi Andrea, Issac,
You can work with just Industrial Comms SDK, now to add IPC project to CCS along with CCS:
1. Import Ethercat project into CCS- This you have already done
2. Import IPC project from the location: ind_comms_sdk_am263x_09_00_00_04\mcu_plus_sdk…
Part Number: MCU-PLUS-SDK-AM243X Tool/software: I use the AM243X Industrial COMMS SDK 09.02.00.09 and I found the LwIP interface source code for ICSS-EMAC doesn't support concatenated pbuf.
In the file am243x-mcu-plus-sdk\source\networking\icss_emac…
Hi Archit,
Thank you for your reply.
I understood that it will be fixed in Industrial Comms SDK v9.2.
We are looking forward to the release of Industrial Comms SDK v9.2.