Part Number: ISO122 What can I expect to see on the output of the ISO122 part when the high side supply goes to ~ 0 Volts but the low side supply is still powered with +15 Volts and -5 Volts?
Part Number: ISO122 Other Parts Discussed in Thread: ISO224 , AMC1411
Hello,
The datasheet mentioned that the ISO 122 is compliant to the VDE0884 standard but does not mention what version (-05, -10, -11, etc.). Knowing which version we tested the…
Part Number: ISO122 Other Parts Discussed in Thread: ISO224 , ISO120 Hi team,
Does TI have any spice model? If not, could you give me comment on if there is alternative product model for ISO122 spice simulation?
Best regards,
Takeshi Sasaki
Part Number: ISO124 Other Parts Discussed in Thread: ISO122 , ISO224 Hello team,
ISO124 seems to have been released after ISO122.
What are the improved characteristics of ISO124 from ISO122? It only looks like the difference in gain non-linearity…
Part Number: ISO122 Hello support team,
I have a question. Could you please teach me the difference between ISO122 and ISO122J.
In the data sheet, it seems that there is only a difference in specification of noise. Is there any other function or characteristic…
Hi Alexander,
Great question! There are some specification differences between the ISO122 P/U vs. JP/JU, please see the top of the Electrical Characteristics table, section 7.5.
Part Number: ISO122 Other Parts Discussed in Thread: ISO224 , AMC1311 Please, answer another question
If I will use ISO122, can I use circuit in attach? Please, see attach.
TIA
Sincerely,
Vladimir Naumenkov
www.agat.by
Isolation amplifier_ISO122…
Part Number: ISO122
Dear sir, please help
I need isolation amplifier (follower) to transfer 1...2V DC voltage. I have two unipolar power supplies +5V-1 and +5V-2. These power supplies isolated from each other. Can I use ISO122? Can you recommend another…