Part Number: ISO3086T Other Parts Discussed in Thread: ISO35T Hello-
I have a customer that migrated away from ADM2487E to ISO3086T. They didn’t realize it is only 5V supply on the bus side.
They are currently giving it 3.3V. They haven’t had any…
Part Number: ISO3086T Hello team,
I received an inquiry from my customer, about RS-485 Transceivers ISO3086T.
Could you confirm the below questions about conflict protections of this IC?
Questions
Is there a protection circuit in place to…
Part Number: ISO3086T Other Parts Discussed in Thread: STRIKE As in EMC testing transience will be applied with reference to non Isolated GND (GND1) is there any method to calculated clamping volttage of TVS connected for protection ?
Also, in…
Part Number: ISO3086T Everywhere in the datasheet Same supply is given to VCC1 and transformer input. Can we apply different supply voltages at VCC1 pin and Transformer input as shown in following Image?
Part Number: ISO3086T Hi Team,
This is a product with a specification upper limit of 50 Mbps. Is there a problem with using at low speed?
My customer wants to use at 9.6 kbps.
This device recognizes that it has not lined up for low speed.
Please…
Part Number: ISO3086T Hi Team,
The customer would like to know if ISO3086T can support RS-485 and RS-422 communication?
Can you confirm this?
Best Wishes, Mickey Zhang Asia Customer Support Center Texas Instruments
Part Number: ISO3086T Hi, Customer wants to use ISO with non-isolation circuit for parts share. Could you give me any advice on the following? 1.Can the circuit described below be realized? Customer is trying to share VDD1/2 and GND1/2. And the transformer…
Part Number: ISO1410 Other Parts Discussed in Thread: ISOW7841 , SN6501 , Hii,
I have a slight doubt of selection of Modbus Isolator
I have to isolate my signal as well as the power-
There are two options i am slecting among
1) ISO1410
in this…
Part Number: ISO3086T Other Parts Discussed in Thread: STRIKE , To whom it may concern,
I was interested in using this part on a current design, but I'm concerned by the following excerpt from the datasheet:
" TI recommends not testing equipment…
Shreyas
We are driving ISO3086T TI Chip. From the datasheet of ISO3086T the drive current on D , R ,DE,RE are 10uA.
Can you please confirm this so that we can close this case ?