Other Parts Discussed in Thread: ISO7220A Hi,All
Let me ask you a question about ISO7220A.
For example , Can I replace ISO7220 with HCPL-M611-560E(AVAGO Inc.) ?
What parameter should I compare ?
Pin compatible is not an important.
I am looking…
Part Number: UCC27714 Other Parts Discussed in Thread: ISO7220A , UCC27714 driving half-bridge LLC converter mosfets. ISO7220A giving pulses to UCC27714 to drive mosfets. initially controller senses input voltage of 400V gives PWM pulses of 250KHZ at…
Hello,
Please take a look at the TIDM-TWOPHASEMETER-I2040 TI Design. This design features a MSP430I2040 as the analog front-end with a MSP430F6638 as the host MCU. You'll notice that there are isolators, specifically ISO7220A and/or ISO7221A, used…
Part Number: ISO7221A-Q1 Other Parts Discussed in Thread: ISO7220A-Q1 , ISO7221C-Q1 , Hi,
"ISO722xC" was eliminated from tsk(o) by revising the datasheet as below.
Could you tell me why?
Best Regards,
Kuramochi
Hi Alexandre, Sorry for the delay in responding. I will also respond to your other post shortly. For this post, I am assuming that you are using the TMDSCNCD28069 (the non-ISO version). This setup is possible. I have some thoughts on it though:
For…
Hello Saleem,
Thank you for your reply.
What's the rating of creepage for ISO7220M after fix the datasheet error?
Is it 4.8mm just like clearance distance?
I found same datasheet error at the below devices.
ISO721
ISO7220A-Q1
ISO7242C…
Carlos Miguel Espinar said: the problem was in the digital isolator ISO7220AC
Hello Carlos,
My board also uses ISO7220A, and I got this solution from the forum
http://e2e.ti.com/support/microcontrollers/c2000/f/171/p/321906/1120577.aspx#1120577…
Problem found and resolved.
In the implementation of the emulator, based on the Experimenter's kit , four optocouplers were added to interface with ControlCARD.
The error was the specification for the optocouplers: ISO7220A (1 Mbps signaling rate…
Brett:
You were riight, it was hardware. We used the wrong version of the ISO7220 chip. We used ISO7220A with a 410ns propogation delay, but TI used the ISO7220C with a 36ns propogation delay. We changed the chips and we were back in the saddle. We…