Part Number: ISO7221C-Q1 Tool/software: Hi,
The datasheet specifies a maximum reverse voltage of 0.5 V for supply and input pins and also a maximum current for the output pin.
This is well understood when looking at the datasheet device I/O diagram…
Part Number: ISO7221C-Q1 Other Parts Discussed in Thread: ISO7331-Q1 , , ISO7321-Q1 , ISO7721-Q1 Hi,
I would like you to confirm meaning of following spec which is described in datasheet.
* 4000-V peak Isolation, 560 V peak VIORM
I believe that…
Hi Koteshwar, Thank you so much for your kind confirmation. Let me introduce the reason and our recommended device must be ISO7221C-Q1 which is the latest. ( I was not able to find ISO7221-Q1 ) ISO1042-Q1 seems the best solution. Thank you for the info…
Hi Kuramochi-san,
As defined in the footnote (3) in the datasheet and also copied below, tsk(o) is the parameter that talks about the difference in propagation delay of two channels that are in same direction. Only ISO7220A-Q1 has two channels in same…
Conor,
I will work to get answers on the above, but our systems and product teams are still largely out for the holiday, so it may take some time to run this down.
As far as I am aware. I do not believe we have a published certificate specifically…
Hi Brian,
Attached is a document which covers what Texas Instruments devices have UL1577 certification as of 6-18-2024. The latest document can be found on the UL website.
In this document you can see the TPSI3052-Q1 covered.
UL1577.pdf
Best Regards…
Hello Mitesh,
Thank you for reaching out to our team's E2E.
You can find the UL certificate for TPSI2072QDWQRQ1 on the UL website at the following link: FPPT2.E181974 - Nonoptical Isolating Devices - Component | UL Product iQ
For your convenience…
Part Number: UCC23513 Hi,
What is the UL number of UCC23513DWYR? Is it number for 20190711-E181974 on the attached file?
Please help to confirm it. Thanks!
sluq004-ucc23513.pdf
Hello Kazuya,
I've attached the certification documents. Additional information about the test method can be found on the UL or VDE website.
In the future, the latest revision of these document should be available under "Technical Documentation" on…
Quickly find solutions to common questions about digital isolator devices by clicking this link. This FAQ answers the most common questions asked about these devices …… ……… …
FAQ: Isolation >> Digital Isolators
Digital Isolators
Isolated Interfaces…