Part Number: ISO7242M Other Parts Discussed in Thread: ISO6742 Hi Team,
Customer want a isolation device use in such a system. Thay want use in a 5Mhz SPI net with all miso connect directly.
So I recommended ISO7242M to him. Customer says he want…
Part Number: ISO7241M Other Parts Discussed in Thread: ISO7231M Hi!
In your data sheet "ISO724x High-Speed, Quad-Channel Digital Isolators",
there is "The signal input pins are 5-V tolerant regardless of the voltage supply level that is used." on…
Hi Masanori,
All the input pins have an absolute max spec of VCC+0.5V that shouldn't be violated to not affect device reliability / lifetime. Any continuous voltage greater than VCC+0.5V at input pins will degrades device's life. Similarly, the lowest…
Part Number: LP-AM243 Other Parts Discussed in Thread: AM4376 , ISO7242M I am trying to evaluate the Intra Drive Communication Using 8b-10b Line Code With Programmable Real Time Unit - Application Note. Will the source code files be made available? That…
Part Number: ISO7240C Tool/software: Hi,
The following items have been changed from revision T (SLLS868T) to revision U (SLLS868U).
• Updated reference from capacitive isolation to isolation barrier throughout the document. →The description "Isolation…
Part Number: ISO7242C-Q1 Other Parts Discussed in Thread: ISO7242C , ISO7242M , ISO6742 Hi ,
We are using ISO7242MDW part in our existing design. However we decided to replace former part with ISO7242CQDWRQ1. I compared parameter and found that both…
Hi TTD,
Thanks for highlighting ISO7242A anomaly. Yes, this is the same anomaly that customer is seeing in their waveform. When a <1µs negative pulse is applied then output gets locked to a LOW state and DC refresh doesn't change the output upto the…
Conor,
I will work to get answers on the above, but our systems and product teams are still largely out for the holiday, so it may take some time to run this down.
As far as I am aware. I do not believe we have a published certificate specifically…