Part Number: L293 Other Parts Discussed in Thread: DRV8844 Hi Team,
We would like to confirm if there is a spice model for this device?
Thank you.
-Mark
Part Number: L293 Hi,
Good Day. I have a customer who is working with L293NE. Please see below his query for your reference. Thank you very much.
The following voltages are applied to L293NE. Pin No. Voltage 1) 5V 2) 3) 4) 0V 5) 0V 6) 7) 23V 8) 23V…
Part Number: L293 Other Parts Discussed in Thread: UCC21222 Hello,
I am designing a DC motor shield using the L293 and am wondering how much electrical isolation it provides, if any, between the MCU and the motor.
Also, are there any recommended…
Part Number: L293 Hi, where can obtain informations about valid marking of the chip L293NE 75CE71M ? The board is assembled externally and I supect a countrefeit because about 3% of mounted chips are not working and the logo and fonts are differents from…
Part Number: ULN2803A
I have this circuit in consideration for a LED display project and I was wondering if a circuit like this would be likely to reduce the longevity of the LED's lifespan, assuming the PWM frequency is high enough to not exceed the…
Other Parts Discussed in Thread: DRV8832 , DRV8833 , DRV8841 , DRV8844 , DRV8843 , DRV8830 Hi,
I am newbie to motor control and I have been tasked to upgrade from a L293B Chip to a PWM chip controlled by a micro.
Looking at the datasheet the L293B…
Part Number: L293 Other Parts Discussed in Thread: DRV8835 , DRV8846
Dear experts,
Customer wants to get feasible driver suitable for step motor they are using.
They need small sized part with similar performance like L293 which was designed in…
Part Number: L293 I want to purchase a L293NE Motor Driver, but I would prefer to get a surface mount package. On this website I only can find the through hole version. Do you guys still sell the surface mount version of the L293NE? Thanks!
Other Parts Discussed in Thread: L293 , DRV8841 , DRV8843 , DRV8844 , DRV8812 , DRV8813 Dear Madam or Sir,
I use L293 as an buffer and level shifter from 5VDC to 24VDC on two of our boards and it works perfectly except for one thing: shorting any…
Other Parts Discussed in Thread: L293 , DRV8808 , DRV8837 , DRV8838 , TLV61046A Hi, i am working with battery powered water flow controller project and i listed the hardware part my design in below,
1. 6V rechargeable battery,
2. IR Transceiver, …