Hello,
I'm not using the ZAP (I prefer starting with the examples) and I've been able to send/receive messages of 600 Bytes without any errors. This is using the stock ZNP hex files. The fragmentation feature is cool but not really well documented…
Other Parts Discussed in Thread: OMAPL138 I am attempting to ulitize the EDMA to loop out data that I have in a 1d array on a OMAPL137. I am getting no activity on the SPI line when I execute my program but if i manually change the data found in SPIDAT1…
Hi Jason, Here is the code. /** ============================================================================
* @n@b Init_Qmss
*
* @b Description
* @n This API initializes the QMSS LLD on core 0 only.
*
* @param[in]
* @n None
*
* @return Int32…
Hi Art,
I'm not sure why the datasheet isn't showing up on the web. I'll look into that to get it fixed.
For now, here's a copy of the document: SN74HCS27-Q1
Hi, IoWave
At present, CC32xx has no reference code about Automatic Baud Rate (ABR) detection. But it has the UART hardware module, you can refer to the document of SLAA215 (Automatic Baud Rate Detection on the MSP430) or the file of bl_autobaud.c as…
Hi Mao-san
Thank you for the reply.
Please let me ask you more detail questions.
1.
I'm sorry. I attached PDF.
Universal Serial Bus Specification.pdf
2.
Does this device flow the current to detect the battery voltage?
How long…
Hi Luis I have one other EVM-U with no LED light on when plugged in. I have followed all the reviving examples. After clearing the EEPROM I do not receive the "new device found" message. I need a suggestion on reviving the EVM. TOM
Hi Gaviraju,
I attached the showconfig output (showconfig.log) and building SDK (VisionSDK_UserGuide_TDA2px.pdf) specifically in Linux Installation section.
Regards
Angel
Fullscreen
3426.showconfig.log
Download
#
# Build Config…
Other Parts Discussed in Thread: TPS25924 We have a question about TPS25924.
We find that recommended footprint of package was changed.
We have old datasheet(attached document).
This is different from datasheet of website about footprint.
Do…